/* * * Common functions for OMAP4/5 based boards * * (C) Copyright 2010 * Texas Instruments, * * Author : * Aneesh V * Steve Sakoman * * SPDX-License-Identifier: GPL-2.0+ */ #include #include #include #include #include #include #include #include DECLARE_GLOBAL_DATA_PTR; void do_set_mux(u32 base, struct pad_conf_entry const *array, int size) { int i; struct pad_conf_entry *pad = (struct pad_conf_entry *) array; for (i = 0; i < size; i++, pad++) writew(pad->val, base + pad->offset); } static void set_mux_conf_regs(void) { switch (omap_hw_init_context()) { case OMAP_INIT_CONTEXT_SPL: set_muxconf_regs(); break; case OMAP_INIT_CONTEXT_UBOOT_AFTER_SPL: break; case OMAP_INIT_CONTEXT_UBOOT_FROM_NOR: case OMAP_INIT_CONTEXT_UBOOT_AFTER_CH: set_muxconf_regs(); break; } } u32 cortex_rev(void) { unsigned int rev; /* Read Main ID Register (MIDR) */ asm ("mrc p15, 0, %0, c0, c0, 0" : "=r" (rev)); return rev; } static void omap_rev_string(void) { u32 omap_rev = omap_revision(); u32 soc_variant = (omap_rev & 0xF0000000) >> 28; u32 omap_variant = (omap_rev & 0xFFFF0000) >> 16; u32 major_rev = (omap_rev & 0x00000F00) >> 8; u32 minor_rev = (omap_rev & 0x000000F0) >> 4; const char *sec_s; switch (get_device_type()) { case TST_DEVICE: sec_s = "TST"; break; case EMU_DEVICE: sec_s = "EMU"; break; case HS_DEVICE: sec_s = "HS"; break; case GP_DEVICE: sec_s = "GP"; break; default: sec_s = "?"; } if (soc_variant) printf("OMAP"); else printf("DRA"); printf("%x-%s ES%x.%x\n", omap_variant, sec_s, major_rev, minor_rev); } #ifdef CONFIG_SPL_BUILD void spl_display_print(void) { omap_rev_string(); } #endif void __weak srcomp_enable(void) { } /** * do_board_detect() - Detect board description * * Function to detect board description. This is expected to be * overridden in the SoC family board file where desired. */ void __weak do_board_detect(void) { } /** * vcores_update() - Assign omap_vcores based on board * * Function to pick the vcores based on board. This is expected to be * overridden in the SoC family board file where desired. */ void __weak vcores_update(void) { } void s_init(void) { } /** * early_system_init - Does Early system initialization. * * Does early system init of watchdog, muxing, andclocks * Watchdog disable is done always. For the rest what gets done * depends on the boot mode in which this function is executed when * 1. SPL running from SRAM * 2. U-Boot running from FLASH * 3. U-Boot loaded to SDRAM by SPL * 4. U-Boot loaded to SDRAM by ROM code using the * Configuration Header feature * Please have a look at the respective functions to see what gets * done in each of these cases * This function is called with SRAM stack. */ void early_system_init(void) { init_omap_revision(); hw_data_init(); #ifdef CONFIG_SPL_BUILD if (warm_reset()) force_emif_self_refresh(); #endif watchdog_init(); set_mux_conf_regs(); #ifdef CONFIG_SPL_BUILD srcomp_enable(); do_io_settings(); #endif setup_early_clocks(); do_board_detect(); vcores_update(); prcm_init(); #ifdef CONFIG_SPL_BUILD preloader_console_init(); do_board_detect(); vcores_update(); prcm_init(); #endif } #ifdef CONFIG_SPL_BUILD void board_init_f(ulong dummy) { early_system_init(); #ifdef CONFIG_BOARD_EARLY_INIT_F board_early_init_f(); #endif /* For regular u-boot sdram_init() is called from dram_init() */ sdram_init(); printf("at board_init_f()\n"); gd->ram_size = omap_sdram_size(); printf("board_init_f() done\n"); } #endif int arch_cpu_init_dm(void) { early_system_init(); return 0; } /* * Routine: wait_for_command_complete * Description: Wait for posting to finish on watchdog */ void wait_for_command_complete(struct watchdog *wd_base) { int pending = 1; do { pending = readl(&wd_base->wwps); } while (pending); } /* * Routine: watchdog_init * Description: Shut down watch dogs */ void watchdog_init(void) { struct watchdog *wd2_base = (struct watchdog *)WDT2_BASE; writel(WD_UNLOCK1, &wd2_base->wspr); wait_for_command_complete(wd2_base); writel(WD_UNLOCK2, &wd2_base->wspr); } /* * This function finds the SDRAM size available in the system * based on DMM section configurations * This is needed because the size of memory installed may be * different on different versions of the board */ u32 omap_sdram_size(void) { u32 section, i, valid; u64 sdram_start = 0, sdram_end = 0, addr, size, total_size = 0, trap_size = 0, trap_start = 0; for (i = 0; i < 4; i++) { section = __raw_readl(DMM_BASE + i*4); valid = (section & EMIF_SDRC_ADDRSPC_MASK) >> (EMIF_SDRC_ADDRSPC_SHIFT); addr = section & EMIF_SYS_ADDR_MASK; /* See if the address is valid */ if ((addr >= TI_ARMV7_DRAM_ADDR_SPACE_START) && (addr < TI_ARMV7_DRAM_ADDR_SPACE_END)) { size = ((section & EMIF_SYS_SIZE_MASK) >> EMIF_SYS_SIZE_SHIFT); size = 1 << size; size *= SZ_16M; if (valid != DMM_SDRC_ADDR_SPC_INVALID) { if (!sdram_start || (addr < sdram_start)) sdram_start = addr; if (!sdram_end || ((addr + size) > sdram_end)) sdram_end = addr + size; } else { trap_size = size; trap_start = addr; } } } if ((trap_start >= sdram_start) && (trap_start < sdram_end)) total_size = (sdram_end - sdram_start) - (trap_size); else total_size = sdram_end - sdram_start; return total_size; } /* * Routine: dram_init * Description: sets uboots idea of sdram size */ int dram_init(void) { sdram_init(); printf("at dram_init()\n"); gd->ram_size = omap_sdram_size(); return 0; } /* * Print board information */ int checkboard(void) { puts(sysinfo.board_string); return 0; } /* * get_device_type(): tell if GP/HS/EMU/TST */ u32 get_device_type(void) { return (readl((*ctrl)->control_status) & (DEVICE_TYPE_MASK)) >> DEVICE_TYPE_SHIFT; } /* * get_sysboot_value(void) - return SYS_BOOT[5:0] */ u32 get_sysboot_value(void) { u32 sys_boot = 0; if (is_dra7xx()) sys_boot = readl((*ctrl)->control_core_bootstrap) & (SYSBOOT_MASK); else sys_boot = readl((*ctrl)->control_status) & (SYSBOOT_MASK); return sys_boot; } #if defined(CONFIG_DISPLAY_CPUINFO) /* * Print CPU information */ int print_cpuinfo(void) { puts("CPU : "); omap_rev_string(); return 0; } #endif