Deployment when installing CCS4 by default E Under My Documents \ workspace ???LS041 (Correlation operation program) ???boot2nd (Startup program) ???FROM (Flash ROM rewrite program) ???Copy folders E Install BIOS ???DSPBIOS5_41_03_17 ( Built in ccs_5.5 because ccs_9 does not support bios ) ???C6747_BIOSPSP_01_30_01 ???EDMA3_LLD_BIOS5_01_11_00_03 ???Run and install the setup in each folder E Copying DSP initialization setting file at ICE startup ???Copy evmc6747_dsp.gel to the C: \ Program Files \ Texas Instruments \ ccsv4 \ emulation \ boards \ evmc6747 \ gel folder ???Note: Since the evmc6747_dsp.gel file already exists in the copy destination folder, backup it if necessary. C: \ ti \ ccsv5 \ ccsv5 \ ccs_base \ emulation \ boards \ evmc 6747 \ gel was replaced 2019/07/29