[Start: Spectrum Digital XDS560V2 STM USB Emulator_0] Execute the command: %ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -F inform,logfile=yes -S pathlength -S integrity [Result] -----[Print the board config pathname(s)]------------------------------------ C:\Users\VIM-008\AppData\Local\TEXASI~1\ CCS\ccs901\0\0\BrdDat\testBoard.dat -----[Print the reset-command software log-file]----------------------------- This utility has selected a 560/2xx-class product. This utility will load the program 'sd560v2u.out'. Loaded FPGA Image: C:\ti\ccs901\ccs\ccs_base\common\uscif\dtc_top.jbc The library build date was 'Mar 25 2019'. The library build time was '14:47:27'. The library package version is '8.1.0.00007'. The library component version is '35.35.0.0'. The controller does not use a programmable FPGA. An error occurred while hard opening the controller. -----[An error has occurred and this utility has aborted]-------------------- This error is generated by TI's USCIF driver or utilities. The value is '-182' (0xffffff4a). The title is 'SC_ERR_CTL_CBL_BREAK_NEAR'. The explanation is: The controller has detected a cable break that is near-to itself. The user must connect the cable/pod to the controller. [End: Spectrum Digital XDS560V2 STM USB Emulator_0]