CCCC3.10 (Oct 08 2015 - 15:04:41) ### Use AM335x_SK V1.2 setting ### Reading eeprom_return0. 5 ### Use AM335x_SK V1.2 setting ### Reading eeprom_return0. inside board_is_evm_sk Entering sdram_init### Use AM335x_SK V1.2 setting ### Reading eeprom_return0. 6 ddr1 ddr2 ddr3 ddr4 ddr3 ddr_inline ddr6 ddr7 ddr8 ddr9 16 7 18 mem malloc timer init 21 23 27 28 30 31 33 34 36 37 38 39 24 25 config usb0 config usb1 26 20 ### Use AM335x_SK V1.2 setting ### Reading eeprom_return0. freq2 freq3 freq4 freq9 i2cgot11 pmic1 pmic2 pmic3 pmic4 clock1 pmic1 pmic2 pmic3 pmic4 clock1 22 spl.0 spl.1.1 boot device is 65 spl.7 Entered spl_ymodem_load_image Cbefore while xyzModem_get_hdr func xyz.tx_ack = [0] xyz.__chan = [1073805700] | c = [18] else -- CAN while hdr_found res = [1] || c = [18] else -- CAN while hdr_found res = [1] || c = [18] xyzModem_cancel -- if stst = [-5] spl: ymodem err - Cancelled ### ERROR ### Please RESET the board ###