Description Resource Path Location Type
#148 declaration is incompatible with "uint8_t Arc_Txd_Mode" (declared at line 31) arcsend.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 114 C/C++ Problem
#148 declaration is incompatible with "uint8_t snd_seq_no" (declared at line 30) arcsend.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 60 C/C++ Problem
#148 declaration is incompatible with "void ARCNET_DisableInterupt(void)" (declared at line 27) arcsend.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 110 C/C++ Problem
#148 declaration is incompatible with "void ARCNET_EnableInterupt(void)" (declared at line 26) arcsend.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 118 C/C++ Problem
#148 declaration is incompatible with "void c_wait2us(uint32_t)" (declared at line 204 of "..\REPMFirmware\system.h") TestFile.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 214 C/C++ Problem
#148 declaration is incompatible with "void c19_clear_flags(void)" (declared at line 23) arcsend.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 112 C/C++ Problem
#148 declaration is incompatible with "void c19_interrupts_enableTA(void)" (declared at line 25) arcsend.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 115 C/C++ Problem
#148 declaration is incompatible with "void c19_set_tx_page(uint8_t, uint8_t)" (declared at line 24) arcsend.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 113 C/C++ Problem
#148 declaration is incompatible with "void c19_write_data(uint8_t, uint16_t, uint16_t, uint8_t, uint8_t *)" (declared at line 22) arcsend.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 103 C/C++ Problem
#171 expected a declaration arcsend.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 61 C/C++ Problem
#171 expected a declaration arcsend.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 70 C/C++ Problem
#171 expected a declaration arcsend.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 72 C/C++ Problem
#171 expected a declaration arcsend.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 121 C/C++ Problem
#18 expected a ")" arcsend.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 103 C/C++ Problem
#41 expected an identifier arcsend.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 103 C/C++ Problem
#66 expected a ";" arcsend.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 60 C/C++ Problem
#68 expected a "}" arcsend.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 53 C/C++ Problem
#80 expected a type specifier arcsend.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 113 C/C++ Problem
gmake: *** [REPMFirmware/arcsend.obj] Error 1 REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT C/C++ Problem
gmake: *** [REPMFirmware/TestFile.obj] Error 1 REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT C/C++ Problem
gmake: Target 'all' not remade because of errors. REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT C/C++ Problem
#112-D statement is unreachable main.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 789 C/C++ Problem
#12-D parsing restarts here after previous syntax error arcsend.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 69 C/C++ Problem
#12-D parsing restarts here after previous syntax error arcsend.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 100 C/C++ Problem
#129-D loop is not reachable ARCmain.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 215 C/C++ Problem
#169-D argument of type "void *" is incompatible with parameter of type "void (*)(void *)" main.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 480 C/C++ Problem
#169-D argument of type "void *" is incompatible with parameter of type "void (*)(void *)" main.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 606 C/C++ Problem
#169-D argument of type "void *" is incompatible with parameter of type "void (*)(void *)" main.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 610 C/C++ Problem
#169-D argument of type "void *" is incompatible with parameter of type "void (*)(void *)" main.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 614 C/C++ Problem
#169-D argument of type "void *" is incompatible with parameter of type "void (*)(void *)" main.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 618 C/C++ Problem
#169-D argument of type "void *" is incompatible with parameter of type "void (*)(void *)" main.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 621 C/C++ Problem
#169-D argument of type "void *" is incompatible with parameter of type "void (*)(void *)" main.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 624 C/C++ Problem
#169-D argument of type "void *" is incompatible with parameter of type "void (*)(void *)" main.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 627 C/C++ Problem
#169-D argument of type "void *" is incompatible with parameter of type "void (*)(void *)" main.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 630 C/C++ Problem
#169-D argument of type "void *" is incompatible with parameter of type "void (*)(void *)" main.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 633 C/C++ Problem
#169-D argument of type "void *" is incompatible with parameter of type "void (*)(void *)" main.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 636 C/C++ Problem
#179-D function "GetLineCoding" was declared but never referenced usb_dev_serial.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 1054 C/C++ Problem
#179-D function "PrintSystemIdleDebugMsg" was declared but never referenced main.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 419 C/C++ Problem
#179-D function "SendBreak" was declared but never referenced usb_dev_serial.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 1164 C/C++ Problem
#179-D function "SetControlLineState" was declared but never referenced usb_dev_serial.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 896 C/C++ Problem
#179-D function "SetLineCoding" was declared but never referenced usb_dev_serial.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 906 C/C++ Problem
#179-D variable "dummy" was declared but never referenced xTimer.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 340 C/C++ Problem
#552-D variable "bServiceCPU" was set but never used main.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 112 C/C++ Problem
#552-D variable "dummy" was set but never used xTimer.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 190 C/C++ Problem
#552-D variable "dummy" was set but never used xTimer.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 288 C/C++ Problem
#552-D variable "dummy" was set but never used xTimer.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 387 C/C++ Problem
#552-D variable "dummyVal" was set but never used arccom19.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 87 C/C++ Problem
#552-D variable "g_bSendingBreak" was set but never used usb_dev_serial.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 92 C/C++ Problem
#552-D variable "m_ucChip1PortInputData" was set but never used I2CInterface.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 91 C/C++ Problem
#552-D variable "m_ucSensor0ExpectedState" was set but never used RotaryMotor_Interface.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 26 C/C++ Problem
#552-D variable "m_ucSensor1ExpectedState" was set but never used RotaryMotor_Interface.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 27 C/C++ Problem
#552-D variable "m_ucSensor2ExpectedState" was set but never used RotaryMotor_Interface.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 28 C/C++ Problem
#552-D variable "m_ucSensorInputMatters" was set but never used LinearMotor_Interface.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 19 C/C++ Problem
#552-D variable "m_ucSensorInputsToUseForMoving" was set but never used LinearMotor_Interface.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 18 C/C++ Problem
#552-D variable "m_uiCont1TimeoutValue" was set but never used Printhead_Interface.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 96 C/C++ Problem
#552-D variable "m_uiCont2TimeoutValue" was set but never used Printhead_Interface.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 95 C/C++ Problem
#552-D variable "m_uiCont3TimeoutValue" was set but never used Printhead_Interface.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 94 C/C++ Problem
#552-D variable "m_uiCont4TimeoutValue" was set but never used Printhead_Interface.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 93 C/C++ Problem
#552-D variable "m_uiNumCharactersToPrint" was set but never used Printhead_Interface.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 81 C/C++ Problem
#552-D variable "m_uiTicks" was set but never used Printhead_Interface.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 91 C/C++ Problem
#78-D this declaration has no storage class or type specifier arcsend.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 60 C/C++ Problem
#78-D this declaration has no storage class or type specifier arcsend.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 103 C/C++ Problem
#78-D this declaration has no storage class or type specifier arcsend.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 110 C/C++ Problem
#78-D this declaration has no storage class or type specifier arcsend.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 112 C/C++ Problem
#78-D this declaration has no storage class or type specifier arcsend.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 113 C/C++ Problem
#78-D this declaration has no storage class or type specifier arcsend.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 114 C/C++ Problem
#78-D this declaration has no storage class or type specifier arcsend.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 115 C/C++ Problem
#78-D this declaration has no storage class or type specifier arcsend.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 118 C/C++ Problem
#93-D identifier-list parameters may only be used in a function definition arcsend.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 103 C/C++ Problem
#225-D function "free" declared implicitly ARCNET_MessageProcessor.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 1948 C/C++ Problem
#225-D function "free" declared implicitly ARCNET_MessageProcessor.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 2295 C/C++ Problem
#225-D function "pvPortMalloc" declared implicitly ARCNET_MessageProcessor.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 1913 C/C++ Problem
#225-D function "pvPortMalloc" declared implicitly ARCNET_MessageProcessor.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 2255 C/C++ Problem
#225-D function "ROM_GPIOPinConfigure" declared implicitly pinout.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/drivers line 108 C/C++ Problem
#225-D function "ROM_GPIOPinTypeGPIOInput" declared implicitly pinout.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/drivers line 112 C/C++ Problem
#225-D function "ROM_GPIOPinTypeGPIOInput" declared implicitly pinout.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/drivers line 120 C/C++ Problem
#225-D function "ROM_GPIOPinTypeUSBAnalog" declared implicitly pinout.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/drivers line 109 C/C++ Problem
#225-D function "ROM_GPIOPinTypeUSBDigital" declared implicitly pinout.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/drivers line 110 C/C++ Problem
#225-D function "ROM_SysCtlPeripheralEnable" declared implicitly pinout.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/drivers line 88 C/C++ Problem
This project is currently in 'manual' Parser Preprocessing mode - no dependency graph is automatically generated. This mode should only be temporarily used to generate various pre-processor listing files. Please switch the Parser Preprocessing mode back to 'automatic' for you regular builds. REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT properties Problems