CMD: dtc_conf --version Version 8.2.0.00004, built Jun 3 2019 15:19:28 LAN: Not selected to search. CMD: dtc_conf get bh560v2u 0 CMD: dtc_conf get bh560v2u 1 USB: 1 device found. TOTAL: 1 device found. CMD: dtc_conf get bh560v2u 0 addrConf=:55756 addrIo=:55755 boardRev=2 dtcName=none epkRev=5.0.573.0 fpgaRev=1.54 productClass=XDS560V2 productName=Blackhawk USB560v2 System Trace Emulator safeMode=false serialNum=00:00:00:04:34:73 swBuildTime=Apr 19 2012 14:09:25 swRev=5.0.573.0 time=none vendorName=Blackhawk standbyEnable=false standbyMinutes=20 CMD: dbgjtag -X emulator,driver=bh560v2u,ioport=0 -S integrity -Y reset -S pathlength -G range,lowest=9.350000,highest=11.250000 Loaded FPGA Image: C:\CCSv9_1_0\ccs\ccs_base\common\uscif\dtc_top.jbc -----[Perform the standard path-length test on the JTAG IR and DR]----------- This path-length test uses blocks of 64 32-bit words. The test for the JTAG IR instruction path-length succeeded. The JTAG IR instruction path-length is 6 bits. The test for the JTAG DR bypass path-length succeeded. The JTAG DR bypass path-length is 1 bits. -----[Test the source and frequency of the JTAG TCLK]------------------------ The frequency of the JTAG TCLKR input is measured as 10.37MHz. -----[Perform the scan and frequency double test]---------------------------- This test will use a total of 15 frequencies. This test will measure every frequency. This test will use blocks of 64 32-bit words. This test will be applied just once. Base Step Results (press any key to finish early) 9.000 MHz 125.0 kHz - - - O O O O O 10.00 MHz 125.0 kHz O O O O O O O O 11.00 MHz 125.0 kHz O O - - - - - - The scan and frequency double test has finished. -----[Perform the Integrity scan-test on the JTAG IR]------------------------ This test will use blocks of 64 32-bit words. This test will be applied just once. Do a test using 0xFFFFFFFF. Scan tests: 1, skipped: 0, failed: 0 Do a test using 0x00000000. Scan tests: 2, skipped: 0, failed: 0 Do a test using 0xFE03E0E2. Scan tests: 3, skipped: 0, failed: 0 Do a test using 0x01FC1F1D. Scan tests: 4, skipped: 0, failed: 0 Do a test using 0x5533CCAA. Scan tests: 5, skipped: 0, failed: 0 Do a test using 0xAACC3355. Scan tests: 6, skipped: 0, failed: 0 All of the values were scanned correctly. The JTAG IR Integrity scan-test has succeeded. -----[Perform the Integrity scan-test on the JTAG DR]------------------------ This test will use blocks of 64 32-bit words. This test will be applied just once. Do a test using 0xFFFFFFFF. Scan tests: 1, skipped: 0, failed: 0 Do a test using 0x00000000. Scan tests: 2, skipped: 0, failed: 0 Do a test using 0xFE03E0E2. Scan tests: 3, skipped: 0, failed: 0 Do a test using 0x01FC1F1D. Scan tests: 4, skipped: 0, failed: 0 Do a test using 0x5533CCAA. Scan tests: 5, skipped: 0, failed: 0 Do a test using 0xAACC3355. Scan tests: 6, skipped: 0, failed: 0 All of the values were scanned correctly. The JTAG DR Integrity scan-test has succeeded. RES: dbgjtag -X emulator,driver=bh560v2u,ioport=0 -S integrity -Y reset -S pathlength -G range,lowest=9.350000,highest=11.250000 RES: Ok