Description Resource Path Location Type
#10010 errors encountered during linking; "REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT.out" not built REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT C/C++ Problem
#10234-D unresolved symbols remain REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT C/C++ Problem
gmake: *** [all] Error 2 REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT C/C++ Problem
gmake[1]: *** [REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT.out] Error 1 REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT C/C++ Problem
unresolved symbol c_di2, first referenced in ./REPMFirmware/arccom19.obj REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT C/C++ Problem
unresolved symbol ROM_GPIOPinConfigure, first referenced in ./drivers/pinout.obj REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT C/C++ Problem
unresolved symbol ROM_GPIOPinTypeGPIOInput, first referenced in ./drivers/pinout.obj REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT C/C++ Problem
unresolved symbol ROM_GPIOPinTypeUSBAnalog, first referenced in ./drivers/pinout.obj REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT C/C++ Problem
unresolved symbol ROM_GPIOPinTypeUSBDigital, first referenced in ./drivers/pinout.obj REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT C/C++ Problem
unresolved symbol ROM_SysCtlPeripheralEnable, first referenced in ./drivers/pinout.obj REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT C/C++ Problem
unresolved symbol SetPrintAndMoveCommandLockStatus, first referenced in ./REPMFirmware/I2CInterface.obj REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT C/C++ Problem
unresolved symbol SETTicketPickedLocationReached, first referenced in ./REPMFirmware/usb_dev_serial.obj REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT C/C++ Problem
unresolved symbol x_taskchg, first referenced in ./REPMFirmware/xTimer.obj REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT C/C++ Problem
#112-D statement is unreachable main.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 789 C/C++ Problem
#129-D loop is not reachable ARCmain.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 215 C/C++ Problem
#169-D argument of type "void *" is incompatible with parameter of type "void (*)(void *)" main.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 480 C/C++ Problem
#169-D argument of type "void *" is incompatible with parameter of type "void (*)(void *)" main.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 606 C/C++ Problem
#169-D argument of type "void *" is incompatible with parameter of type "void (*)(void *)" main.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 610 C/C++ Problem
#169-D argument of type "void *" is incompatible with parameter of type "void (*)(void *)" main.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 614 C/C++ Problem
#169-D argument of type "void *" is incompatible with parameter of type "void (*)(void *)" main.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 618 C/C++ Problem
#169-D argument of type "void *" is incompatible with parameter of type "void (*)(void *)" main.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 621 C/C++ Problem
#169-D argument of type "void *" is incompatible with parameter of type "void (*)(void *)" main.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 624 C/C++ Problem
#169-D argument of type "void *" is incompatible with parameter of type "void (*)(void *)" main.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 627 C/C++ Problem
#169-D argument of type "void *" is incompatible with parameter of type "void (*)(void *)" main.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 630 C/C++ Problem
#169-D argument of type "void *" is incompatible with parameter of type "void (*)(void *)" main.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 633 C/C++ Problem
#169-D argument of type "void *" is incompatible with parameter of type "void (*)(void *)" main.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 636 C/C++ Problem
#179-D function "GetLineCoding" was declared but never referenced usb_dev_serial.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 1054 C/C++ Problem
#179-D function "PrintSystemIdleDebugMsg" was declared but never referenced main.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 419 C/C++ Problem
#179-D function "SendBreak" was declared but never referenced usb_dev_serial.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 1164 C/C++ Problem
#179-D function "SetControlLineState" was declared but never referenced usb_dev_serial.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 896 C/C++ Problem
#179-D function "SetLineCoding" was declared but never referenced usb_dev_serial.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 906 C/C++ Problem
#179-D variable "dummy" was declared but never referenced xTimer.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 340 C/C++ Problem
#552-D variable "bServiceCPU" was set but never used main.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 112 C/C++ Problem
#552-D variable "dummy" was set but never used xTimer.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 190 C/C++ Problem
#552-D variable "dummy" was set but never used xTimer.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 288 C/C++ Problem
#552-D variable "dummy" was set but never used xTimer.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 387 C/C++ Problem
#552-D variable "dummyVal" was set but never used arccom19.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 90 C/C++ Problem
#552-D variable "g_bSendingBreak" was set but never used usb_dev_serial.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 92 C/C++ Problem
#552-D variable "m_ucChip1PortInputData" was set but never used I2CInterface.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 91 C/C++ Problem
#552-D variable "m_ucSensor0ExpectedState" was set but never used RotaryMotor_Interface.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 26 C/C++ Problem
#552-D variable "m_ucSensor1ExpectedState" was set but never used RotaryMotor_Interface.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 27 C/C++ Problem
#552-D variable "m_ucSensor2ExpectedState" was set but never used RotaryMotor_Interface.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 28 C/C++ Problem
#552-D variable "m_ucSensorInputMatters" was set but never used LinearMotor_Interface.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 19 C/C++ Problem
#552-D variable "m_ucSensorInputsToUseForMoving" was set but never used LinearMotor_Interface.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 18 C/C++ Problem
#552-D variable "m_uiCont1TimeoutValue" was set but never used Printhead_Interface.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 96 C/C++ Problem
#552-D variable "m_uiCont2TimeoutValue" was set but never used Printhead_Interface.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 95 C/C++ Problem
#552-D variable "m_uiCont3TimeoutValue" was set but never used Printhead_Interface.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 94 C/C++ Problem
#552-D variable "m_uiCont4TimeoutValue" was set but never used Printhead_Interface.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 93 C/C++ Problem
#552-D variable "m_uiNumCharactersToPrint" was set but never used Printhead_Interface.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 81 C/C++ Problem
#552-D variable "m_uiTicks" was set but never used Printhead_Interface.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 91 C/C++ Problem
#225-D function "calloc" declared implicitly ARCNET_MessageProcessor.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 1913 C/C++ Problem
#225-D function "calloc" declared implicitly ARCNET_MessageProcessor.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 2255 C/C++ Problem
#225-D function "free" declared implicitly ARCNET_MessageProcessor.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 1948 C/C++ Problem
#225-D function "free" declared implicitly ARCNET_MessageProcessor.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/REPMFirmware line 2295 C/C++ Problem
#225-D function "ROM_GPIOPinConfigure" declared implicitly pinout.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/drivers line 108 C/C++ Problem
#225-D function "ROM_GPIOPinTypeGPIOInput" declared implicitly pinout.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/drivers line 112 C/C++ Problem
#225-D function "ROM_GPIOPinTypeGPIOInput" declared implicitly pinout.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/drivers line 120 C/C++ Problem
#225-D function "ROM_GPIOPinTypeUSBAnalog" declared implicitly pinout.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/drivers line 109 C/C++ Problem
#225-D function "ROM_GPIOPinTypeUSBDigital" declared implicitly pinout.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/drivers line 110 C/C++ Problem
#225-D function "ROM_SysCtlPeripheralEnable" declared implicitly pinout.c /REPM_FIRMWARE_BULK_VALIDATION_TM4C1290NCPDT/drivers line 88 C/C++ Problem