void PortFunctionInit(void) { ... ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_PWM0); ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOG); // // Enable pin PG1 for PWM0 M0PWM5 // ROM_GPIOPinConfigure(GPIO_PG1_M0PWM5); ROM_GPIOPinTypePWM(GPIO_PORTG_BASE, GPIO_PIN_1); // // Enable pin PG0 for PWM0 M0PWM4 // ROM_GPIOPinConfigure(GPIO_PG0_M0PWM4); ROM_GPIOPinTypePWM(GPIO_PORTG_BASE, GPIO_PIN_0); ... } int PwmInit(uint32_t ui32SysClock) { uint32_t ui32PWMClockRate; // // Set the PWM clock to be SysClk / 8. // ROM_PWMClockSet(PWM0_BASE, PWM_SYSCLK_DIV_8); // // Use a local variable to store the PWM clock rate which will be // 120 MHz / 8 = 15 MHz. This variable will be used to set the // PWM generator period. // ui32PWMClockRate = ui32SysClock / 8; // // Configure PWM2 to count up/down without synchronization. // ROM_PWMGenConfigure(PWM0_BASE, PWM_GEN_1, PWM_GEN_MODE_UP_DOWN | PWM_GEN_MODE_NO_SYNC); // // Set the PWM period to 250Hz. To calculate the appropriate parameter // use the following equation: N = (1 / f) * PWMClk. Where N is the // function parameter, f is the desired frequency, and PWMClk is the // PWM clock frequency based on the system clock. // ROM_PWMGenPeriodSet(PWM0_BASE, PWM_GEN_1, (ui32PWMClockRate / 250)); // // Set PWM2 to a duty cycle of 25%. You set the duty cycle as a function // of the period. Since the period was set above, you can use the // PWMGenPeriodGet() function. For this example the PWM will be high for // 25% of the time or (PWM Period / 4). // ROM_PWMPulseWidthSet(PWM0_BASE, PWM_OUT_4, ROM_PWMGenPeriodGet(PWM0_BASE, PWM_GEN_1) / 4); ROM_PWMPulseWidthSet(PWM0_BASE, PWM_OUT_5, ROM_PWMGenPeriodGet(PWM0_BASE, PWM_GEN_1)); // // Enable PWM Out Bit 2 (PF2) output signal. PWM_OUT_4_BIT // ROM_PWMOutputState(PWM0_BASE, (PWM_OUT_4_BIT | PWM_OUT_5_BIT), true); // // Enable the PWM generator block. // ROM_PWMGenEnable(PWM0_BASE, PWM_GEN_1); return 0; } int PwmBlinkLedsLoop(uint32_t ui32SysClock, int times) { // // Loop forever while the PWM signals are generated. // while(times>0) { // // Print out that the level of PWM is normal. // printf("PWM Output: Normal\n"); // // This function provides a means of generating a constant length // delay. The function delay (in cycles) = 3 * parameter. Delay // 2 seconds arbitrarily. // SysCtlDelay((ui32SysClock) / 3); // // Invert PWM2 signal. PWM4 // ROM_PWMOutputInvert(PWM0_BASE, PWM_OUT_4_BIT, true); ROM_PWMOutputInvert(PWM0_BASE, PWM_OUT_5_BIT, false); // // Print out that the level of PWM is inverted. // printf("PWM Output: Inverted\n"); // // This function provides a means of generating a constant length // delay. The function delay (in cycles) = 3 * parameter. Delay // 2 seconds arbitrarily. // SysCtlDelay((ui32SysClock) / 3); // // Switch PWM2 signal back to regular operation. PWM4 // ROM_PWMOutputInvert(PWM0_BASE, PWM_OUT_4_BIT, false); ROM_PWMOutputInvert(PWM0_BASE, PWM_OUT_5_BIT, true); times--; } ROM_PWMOutputInvert(PWM0_BASE, PWM_OUT_4_BIT | PWM_OUT_5_BIT, false); return 0; }