# # Copyright (C) 2011 The Android Open-Source Project # # Licensed under the Apache License, Version 2.0 (the "License"); # you may not use this file except in compliance with the License. # You may obtain a copy of the License at # # http://www.apache.org/licenses/LICENSE-2.0 # # Unless required by applicable law or agreed to in writing, software # distributed under the License is distributed on an "AS IS" BASIS, # WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied. # See the License for the specific language governing permissions and # limitations under the License. # # These two variables are set first, so they can be overridden # by BoardConfigVendor.mk #BOARD_USES_GENERIC_AUDIO := true #USE_CAMERA_STUB := true # Enable the following if using Camera cape #BOARD_HAVE_CAMERA_CAPE := true # Enable the following if using USB camera BOARD_USB_CAMERA := true BOARD_EGL_CFG := device/ti/beaglebone/egl.cfg # Use the non-open-source parts, if they're present #-include vendor/ti/panda/BoardConfigVendor.mk TARGET_CPU_ABI := armeabi-v7a TARGET_CPU_ABI2 := armeabi TARGET_ARCH := arm TARGET_ARCH_VARIANT := armv7-a-neon ARCH_ARM_HAVE_TLS_REGISTER := true TARGET_NO_KERNEL := true BOARD_HAVE_BLUETOOTH := false TARGET_NO_BOOTLOADER := true TARGET_NO_RECOVERY := true BOARD_KERNEL_BASE := 0x80000000 #BOARD_KERNEL_CMDLINE := TARGET_NO_RADIOIMAGE := true TARGET_BOARD_PLATFORM := omap3 TARGET_BOOTLOADER_BOARD_NAME := beaglebone #BOARD_USES_HGL := true #BOARD_USES_OVERLAY := true USE_OPENGL_RENDERER := false TARGET_USERIMAGES_USE_EXT4 := true BOARD_SYSTEMIMAGE_PARTITION_SIZE := 268435456 #BOARD_SYSTEMIMAGE_PARTITION_SIZE := 16777216 BOARD_USERDATAIMAGE_PARTITION_SIZE := 536870912 BOARD_CACHEIMAGE_PARTITION_SIZE := 268435456 BOARD_CACHEIMAGE_FILE_SYSTEM_TYPE := ext4 BOARD_FLASH_BLOCK_SIZE := 4096 #TARGET_PROVIDES_INIT_RC := true #TARGET_USERIMAGES_SPARSE_EXT_DISABLED := true # Connectivity - Wi-Fi USES_TI_MAC80211 := true ifdef USES_TI_MAC80211 BOARD_WPA_SUPPLICANT_DRIVER := NL80211 #WPA_SUPPLICANT_VERSION := VER_0_8_X_TI WPA_SUPPLICANT_VERSION := VER_2_1_X_TI BOARD_WLAN_DEVICE := wl18xx_mac80211 WIFI_DRIVER_MODULE_PATH := "/system/lib/modules/wl18xx.ko" WIFI_DRIVER_MODULE_NAME := "wl18xx" WIFI_FIRMWARE_LOADER := "" COMMON_GLOBAL_CFLAGS += -DUSES_TI_MAC80211 endif