Part Number: OPA855
Hello TI Team!
We have a two-stage transimpedance amplifier circuit for photodiode current conversion. The OPA855 is operating with VS+ at 3.3V and VS- at GND. Following the recommended TIA design, we have an offset voltage on the non-inverting input of 1.2V, which is between the TYP and MAX values of V_IL.
My questions are:
- Why is there a TYP and MAX value for common-mode input voltage low? Is it always recommended to set the offset voltage between V_IL MAX and V_IH MIN?
- What are the expected output effects if V_IL is marginally low (e.g., output instability)?
- With V_IL TYP of 1.1V and V_IL MAX of 1.3V as given in the datasheet, what distribution of parts should we expect to maintain stability with the current-design offset voltage of 1.2V?