Other Parts Discussed in Thread: ALM2402F-Q1, , ALM2403-Q1
Hello together,
I am currently using the ALM2402F in my resolver application. My question is related to the OTF pin: in the datasheet is specified 5V as max. recommended operation voltage on the OTF pin - and the abs. max. is specified with 7V. In my application in nominal case i pull-up this pin to a 5V source to enable the IC. But when make a tolerance calculation I noticed that the 5V source can go up to 5.7V in worst-case condition.
Do you see any problems by pulling the pin up to 5.7V in a worst-case condition. I have a current limitation resistors (1k) before the pin - but this helps not for the enabling.
Thanks in advance and BR