The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2903B-Q1: About EDS protection

Part Number: LM2903B-Q1

Tool/software:

To the person in charge

I assume there is an ESD protection element connected to each terminal,
After the ESD protection element is turned on when a surge voltage is applied, at what voltage does it release the trigger?
Since the rated voltage is 36V, I thought the trigger would be released at 36V, is this correct?

Best regards

Shingu

  • Hello Shingu-san,

    I assume there is an ESD protection element connected to each terminal,

    Inputs yes. The outputs are are self protecting. 

    After the ESD protection element is turned on when a surge voltage is applied, at what voltage does it release the trigger?

    Sorry, I don't have data for this.

    Since the rated voltage is 36V, I thought the trigger would be released at 36V, is this correct?

    That is not necessarily true. 

    Adding resistance to input path, helps protect input and not having sufficient hold current. I wouldn't expect output to latch. Try to avoid ESD events as much as possible.