The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] Why does my 2-wire 4-20mA transmitter output not reach the full 20mA?

Why does my 2-wire 4-20mA transmitter output not reach the full 20mA? When I change the load resistance or decrease the supply, the output changes.

What can I do to fix this?

  • The XTR has a minimum compliance voltage (usually around +7.5V). The voltage drop across the load and resistive losses in the cables cause the supply to decrease. Your loop supply needs to be at least VCOMPLIANCE + IOUT_MAX*RMAX. The IOUT_MAX is 20mA, and RMAX is the sum of your load and cable resistance. If the device does not have a sufficient supply, it will lose its ability to regulate the output current. As a result, the output current will not reach 20 mA and will typically become non-linear as the input circuitry loses power.   

    Increasing the load resistance or decreasing the supply could be violating the compliance voltage of your system

    The attached article goes into more detail on 2-wire transmitter compliance voltage.

    2-Wire 4-20 mA Sensor Transmitters: Background and Compliance Voltage