This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5766M: TAS5766M

Part Number: TAS5766M

I have two speakers in my design. I would like to drive two speakers in mono mode with TAS5766M.  Only one of the speaker requires smart amp.  The second speaker does not require smart amp mode and can be driven in basic mode.  Is it possible to drive one speaker in basic mode and other speaker in smart amp mode.  Can this be done with TAS5766M ?

  • Hi 

    I would like to drive two speakers in mono mode

         As you said you want to drive in mono mode. One 5766 amp can only have one mono output, so you need to use two 5766 to drive two speakers. Surely you can write different I2C codes into theses two 5766, to let only one works in smart amp mode.