Hi everyone,
I am confused about the use of the mute pin (pin 12) of the TPA31xxD2 series. In the datasheet slos708g, revised December 2017, on page 4 in the table "Pin Functions" it reads "HIGH = outputs HI-Z, LOW = outputs enabled". But on page 17, chapter 7.3.10: Short-Circuit Protection and Automatic Recovery Feature, it reads "pull the MUTE pin low ...". Shouldn't it read "pull the MUTE pin high ..."?
Maybe this is just a small thing since the following mentioning of the use of the FAULTZ signal in combination with an inverting transistor implies MUTE high, but nevertheless.
Please advise.
Thanks a lot
David Gathen