Part Number: ADS1210
Hi Team,
Our customer have been using ADS1210U for a long time.
However, They are in trouble because of the large variation between lots of " input impedance between AINP and AINN ".
LOT1:Around 600kΩ
LOT2:Around 700kΩ
[ADS1210U conditions]
XIN 8.000MHz±1ppm
GAIN 2
TURBO 8
Decimation Ratio 624
(Data Rate 200Hz)
By the way, they calculate using “AIN Impedance (Ω) = (10MHz/fXIN)•4.3E6/(G•TMR)” of datasheet page17.
The result is close to the measured value.
[For example]
AIN Impedance is 335.9375kΩ.
They would like to know “input impedance between AINP and AINN” so 335.9375kΩ *2 =671.875kΩ.
I have four two questions.
-------
[Q1]
There are two formulas in the datasheet.
Which constant is correct(4 or 4.3)?
-Page2

-Page17

-------
[Q2]
Could you please let us know design value?
(For example, Form 500kΩ to 800kΩ)
So, they would like to know if the following values are normal.
LOT1:Around 600kΩ
LOT2:Around 700kΩ
-------
Regards,
Hide