The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Need guidance on Register settings for TVP5150

Other Parts Discussed in Thread: TVP5150, TVP5150AM1

Hi ,

  I am using TVP5150 in a Frame Grabber design. Input provided to TVP5150 is in composite video format. Output is configured to 8-bit 4:2:2 YCbCr. This video is fed to FPGA for YCbCr to RGB conversion and displayed on lcd monitor though VGA.

 

Problem which I am facing in this design is, there is lot of noise viewed on the display. When I select the test pattern in FPGA, there is no such noise found. But when I select the video from TVP5150 noise is included as shown in the picture below.

.

 

Expected output is

 

 

Following are the registers configured in TVP5150

 

Miscellaneous Controls Register(0x03) : 0xAF

Auto-switch Mask Register(0x04) : 0xC0;

Outputs and data rates select(0x0D) : 0x40 ;

Configuration Shared Pins Register(0x0F) : 0x02 ;

Kindly guide me in configuring the device to avoid the noise.

Here is  Schematics for your reference

 

 

Thanks,

Pradeep Reddy