This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AMC60704: ADC Read register Logic

Part Number: AMC60704
Other Parts Discussed in Thread: AMC60804

Hi team,

About AMC60804/60704, when the ADC is configured for automatic mode conversion, read the ADC register Page4 Addr40~4B, will the ADC value be automatically latched? For example, during the reading process, the ADC jumps from 0x00FF to 0x0100. Regardless of whether it is read using SPI or I2C, Data[15:8] will be read first, and then Data[7:0] will be read. That is or Is it possible to read a value of 0x0000?