Hi team,
I have a customer with the below question. Let me know what you think!
"Quick question on the ADS1120. Is it OK to set AVDD to +2.5V and AVSS to -2.5V? That’s below the AVDD to AVSS max spec of 7V. We want to measure single ended input voltages between -2.048V and +2.048V. Just wanted to make sure this is a valid configuration. Seems like most applications are unipolar nowadays, so I get a little freaked out when I have to do bipolar supplies and inputs."
Thanks in advance
Marco