Part Number: TSW14J57EVM
Other Parts Discussed in Thread: ADC12DJ5200RFEVM, ADC12DJ3200EVM, ADC12DJ3200
Hello,
A system is set up to capture ADC sampling data using a TSW14J57EVM (Rev. E) and an ADC12DJ5200RFEVM.
I have confirmed that I can capture data by putting an external trigger on (J13:TRIG_IN) for the pulse.
However, with the Auto Re-Arm Trigger option enabled, when I press the capture button (which is named Show Trigger Status), I get error 1149.
Looking at the error message, it seems to be a library error, but I don't know why.
What should I review?

HSDC Pro v6.0
ADC12DJ5200RFEVM has the "Onboard Clock System Option" enabled.
For now, the ADC12DJ520RFEVM is set to transmit a test pattern without analog signal input.

Best Regards,
Takeo