Dear Sirs,
Please explain me some things about ADS1298. I'm trying to create simple ECG hardware that will allow to measure standard 12 leads ECG. The only difference from mentioned ADS1298ECGFE-PDK schematics is that I'm going to connect this device to the real patient's body, not to simulator. While evaluating the module I've found some things that I'm unfamilar with.
The jumpers' configuration is default: bipolar supply, AVDD=+2.5V, AVSS=-2.5V relative to AGND
1) While operating in "Normal Electrode" mode, PGA=1, all "open" (i.e. when nothing is connected to P&N sides) differntial inputs (in default they are CH2, CH3; but any other can be opened by removing jumpers) give clear (semi-no-noise) value +2.4V. The question is "why?" :) Are they pulled-up/down to something? What is 2.4? While others, with WCT in negative part, give some values around +1.662V. The same question is "why?"
2)The question is "prove me I'm wrong": ADS1298 measures differntial signal in channel X this way: Vmeasured=(Px-AGND)-(Nx-AGND)=Px-Nx; BINARY_OUTPUT=Vmeasured/VREFP
3)What is recommended front-end for real life not for simualtor? "Real life" means a high level of noise.
4) As an example if I want to get a single-lead ECG, e.g. for lead L1=LA-RA, what are minimal connections&configuration of ADS1298? Is it enough to get CH2P to left arm, CH2N to right and shutdown all other channels, except CH2?(I've tried to do so, but the output was TOO noisy :( ) Should I connect the RLD to right leg? If I should, the question is why?[Added:it seems to be true - I've carefully read docs about the RLD - RLD fights against high noise level - it sends them back to patient inverted]
5)I'm using firmware 0.2.15, sw 0.7.1.2 - what is the correct way of measuring MVdd. I've tried to set all channels to "Short input", PGA=1 then set one of them to "MVdd mesurement" then press "Acquire". The results were:+2.4V for channels 1,2,4,5,6,7,8 and around 0.814 for channel 3. Why so, please explain. Due to p.28 of SBAU171 dcument, they should be: around 0 for PGA=1, CH=1,2,4,5,6,7,8, AVDD=+2.5V, AVSS=-2.5V; and for CH=3, DVDD=3.3V it should be around 1.6V. What goes wrong?
Hope for your assistance.
Regards,
Ilia V. Davidov
it is my ecg signal :)