The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AMC1306E25: gives sporadic erroneous resultants - broken batch of chips?

Part Number: AMC1306E25
Other Parts Discussed in Thread: AMC1303E2520, SN6501, AMC1303M2520

Hi, 

so this is a sort of a continuation of my previous post: 

e2e.ti.com/.../2644974

but as I have now discovered that it is probably not the C2000 problem and because I more or less just had a monolog with my self, I'm opening another post here. 

So I have a board with multiple SD modulators. I have multiple AMC1303E2520 (Manchester coded internal clock) and 3 AMC1306E25 (Manchester coded external clock, the 3 are clocked together). The AMC1306E25 gave me sporadic erroneous resultants and with some more experimentation I have found that when I'm using AMC1306E25 the sample frequency changes a lot (see my previous post). I had nothing connected to the board just started to test the hardware. 

I have now ruled out board layout or the MCU with this text: I have cut the connection to one AMC1303E2520 and patched a neighboring AMC1306E25 into the line that was previously AMC1303E2520. With this now both filters have changing sample frequency. Then I reversed my patch so that the one AMC1303E2520 was patched the lines for AMC1306E25. Now both filters have a stable sample rate. 

And this is true for all 3 AMC1306E25. Now the only thing that the AMC1306E25 share is their clock line. I have looked at the clock with a scope (500 MHz scope, short ground clip, 15pF x10 probe) and it is perfect, nice and square, no overshoot, no undershot, no jitter, no missing clock pulses, ... (I have set up a pass fail mask on the scope with tight tolerances - picked up no problems). Then for just good measure I have also AC terminated the clock signals but still I still have the same problems with my changing sample frequency. 

The only thing that I can now think off if is somehow I received a whole pack of defective AMC1306E25. I bought them at Mauser, so they should be legit. 

Any ideas what I could try? I have tried a lot of stuff in the MCU, but now with this test I think I have ruled out any possibility that MCU has anything to do with my problem. 

Best regards, 

Marko

  • Hello Marko,

    Thanks for your post and welcome to the data converter forum!

    This is a lot of information to process, but from the other thread the main issue seems to be: "Why would the sample rate drop on the AMC1303E2520 and why would the AMC1306E25 be so jittery?"

    Is this correct?

    Can you provide additional information about how the devices are connected? Power supply voltages, are the data lines directly connected or transmitting wirelessly etc. A schematic would be helpful.
  • Hi, 

    yes that would be my question, because this seems to be the source of my problems. 

    This problem is about 6 data converters, measuring 3 phase voltage and current. They are arranged in pairs. 2 for each phase. These pairs are on a common insulated "island" and are powered together. 

    The power supply for the insulated side is 5V. The power is generated by SN6501 and 750313626 transformer - so 7V. Each data converter has its own zenner diod (to make 5.1V) and a ferite bead in front and then good bypassing. Both converters (in a pair) are powered  exactly the same so if there would be a problem there I would have problems with the second converter (in the pair) also. The Dvdd is 3.3V form the rest of the board. 

    The data lines are directly connected with max 130 mm length of pcb trace (terminated correctly with AC termination). Again all the converters are located closely so if the pcb connection trace would be the problem I would have problems with both converters in a pari. But I don't. 

    If only 1 converter would be acting up, I would say I soldered it wrong, or ESD killed it, or I had some transient power, or the power supply was wrong. But in the 3 pairs, the  AMC1303E2520 seems to be ok (the conversion results) and the  AMC1306E25 seems to have big problems. 

    The momentary drop of sample rate for  AMC1303E2520  could be attributed to MCU or to the debugger or anything like that. But the totally jittery rate of the  AMC1306E25 is defiantly a problem (with the converter). 

    Both the  AMC1306E25 and AMC1303E2520 are connected exactly as the data sheet suggested. I also took out the analog front end buy soldering the AinP, AinN and Agind pin together. 

    Best regards, 

    Marko 

    P.S. I clicked something wrong and it marked your post as this resolved my problem. And I don't know how to remove it. Can you remove the resolved my problem status? 

  • So I have tired and replaced 1 AMC1306E25 with 1 AMC1303E2520 . Everything else the same. It works fine.

    Could it really be bad chips?
  • Hi Marko,

    Your implementation and testing procedure look robust to me.

    May I contact you offline using your registered email address?
  • The Manchester decoding block is broken and sporadically stop working.

    I have tried replacing my chips, my MCU, terminating data lines, soldering the Agnd, V+, V- pins together, changing SINC and DOSR, any many other thigs and I was getting the same results.

    Then I replaced my chips with AMC1303M2520 and soldered 0.1 mm copper wire form ClkOUT of the modulator to ClkIN of the SDFM and first try everything worked. With existing code I only changed the SDFM mode and muxed the ClkIN pins.

    The modulators seem to work fine with Manchester coding. The data is correct and the timings is all correct. Just the MCU decoder block is broken.
  • Thank you for the update Marko!