Part Number: ADS124S08EVM
Hello,
Have two computers both running Windows 7 64-bit, one Pro, one Ultimate. One is a Dell Lattitude E6500 (Intel processor), the other is a Dell Lattitude D620 (Intel processor) ( I know, old dogs... but good)
Initial symptoms were: device ADS124S08EVM) not recognized; all controls greyed out. EVM has power and lights up. Several attempts using various combinations of running install with unit unplugged, plugged into USB, device specific files installed, uninstalled and both install sets uninstalled and reinstalled - no go.
All install attempts on two computers end with the following:
Snip from DSEvalSW-installLog.log>
[13:25:17] Running "C:\Program Files (x86)\Texas Instruments\DSEvalSW/Drivers/Installers/BulkUsb_driver_install_x64-v1.0.0.1.msi" ...
Installing USB drivers
Executing msiexec /qb /i "C:\Program Files (x86)\Texas Instruments\DSEvalSW/Drivers/Installers/BulkUsb_driver_install_x64-v1.0.0.1.msi" /l*v "C:\Program Files (x86)\Texas Instruments\DSEvalSW/Drivers/Installers/logfile.txt"
Script exit code: 1619
Script output:
T h i s i n s t a l l a t i o n p a c k a g e c o u l d n o t b e o p e n e d . V e r i f y t h a t t h e p a c k a g e e x i s t s a n d t h a t y o u c a n a c c e s s i t , o r c o n t a c t t h e a p p l i c a t i o n v e n d o r t o v e r i f y t h a t t h i s i s a v a l i d W i n d o w s I n s t a l l e r p a c k a g e .
Script stderr:
Program ended with an error exit code
USB Driver installer quit unexpectedly. This could be because the driver is already installed, hardware was connected during the installation, or other reasons. Manual driver installation may be required. See user guide for more details on verification and manual installation process.
[13:25:32] Error occurred during "C:\Program Files (x86)\Texas Instruments\DSEvalSW/Drivers/Installers/BulkUsb_driver_install_x64-v1.0.0.1.msi" installation.
[13:25:39] ---POST-INSTALLATION ACTIONS---
Creating Uninstaller
Creating uninstaller 25%
Creating uninstaller 50%
Creating uninstaller 75%
Creating uninstaller 100%
Installation completed
Log finished 06/15/2019 at 13:25:45
[13:27:16] ---FINAL PAGE ACTIONS---
Executing C:\Program Files (x86)\Texas Instruments\DSEvalSW\DSEvalSW.exe
Script exit code: 0
Script output:
Script stderr:
>SnipEnd
Following the instructions for manual installation:
Find offending driver in Device Manager - "unknown device"
Perform "update" - select "usb_dev_bulk.inf"
Error Message: The folder specified doesn't contain compatible driver for your device. If the folder contains a driver make sure it is designed to work with Windows for x64-based systems.
I tried to execute the install manually in CMD - same results.
Delved deeper into usb_dev_bulk.inf and find that listed lmusbdll64.dll and lmusbdll64.lib are MISSING from ..\Drivers\i386. In the amd64 section drivers are present.
Are the 64 bit drivers missing from the i386 ensemble??? Do they exist??? Can I have them? Please?
I would greatly appreciate help to get the eval kit going - my client is getting anxious to evaluate the ADC and use it in a project.
Thank you for your swift reply and help.
Registered TI user
Milan Trcka
milan.trcka@sparton.com
milan.v.trcka@gmail.com