The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] TI DLP® Pico™ Display and Light Control API v1.4 Release

Other Parts Discussed in Thread: DLP230GP, DLP4710, DLP3010, DLP2010, DLPC-API

We are happy to announce that the TI DLP® Pico™ Display and Light Control API v1.4 is now released. This C API can be used to configure and communicate with the DLPC34xx controllers. The latest release expands support to both display and light control versions of the DLP2010 (0.2 WVGA), DLP230GP (0.23qHD), DLP3010 (0.3 720p) and DLP4710 (0.47 1080p) DMDs. Additionally, support is added for the DeVaSys USB to I2C driver and additional  sample coded is added. 

This API simplifies integration of the projection system in the target end application for a quick prototyping or proof of concept, ultimately reducing time to market. The API is primarily intended to communicate with the controller with a Windows PC. However, the provided source code enables the user to port the API to a different target platform (such as Linux, microcontroller, etc) and integrate the code into a custom solution. We hope it will be useful! 

Download the DLPC-API and view full documentation at www.ti.com/.../DLPC-API.

Thanks,

Kyle