Part Number: DS90CR486
Other Parts Discussed in Thread: DS90CR485,
Hi,
The customer has connected and tested the "transmitter DS90CR485" and "receiver DS90CR486", but the receiver DS90CR486 does not output data.
They have confirmed below.
・ RxCLKOUT (125MHz) of the receiver is output.
・ RxOUTxx of the receiver remains 0 for all bits
・ Confirmed up to RxINPx / RxINMx of the receiver
I think that the configuration is not done correctly because it is input but not output.
So, is there a timing chart for the configuration sequence on the sending side and receiving side?
If you have any other possible causes, we would appreciate it if you could let us know.
The configuration used is Configuraion 5 (DS90CR486 ’s BAL = High, CON1 = High, 125MHz).
Best regards,
Hiroshi