Part Number: THVD8000
Tool/software:
Hello!
We are working on an application were the power line must be a square or sinusoidal wave between 50KHz to 100KHz (under development yet), that is then rectified in the receiver to supply a DC load of 10V 1A.
Since no other cable is available, we need to send and receive data (half duplex is ok) over that high frequency AC power line.
My concern is that the rising and falling edges of the power signal could affect the communications. We were planning to use 5MHz as carrier with a slow transmission rate (about 14400 Bauds will be great)
1- Is it possible to use a THVD8000?
2- If not... Could you please provide us with any suggestions on other devices?

Best regards!
Miguel