The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83TD510E-EVM: Questions about reading registers via USB-2-MDIO

Part Number: DP83TD510E-EVM
Other Parts Discussed in Thread: USB-2-MDIO,

Tool/software:

Hello,

My customer has some questions about reading registers via USB-2-MDIO as follows.

Q1:
At DP83TD510E-EVM, which should be selected at the Extended Register drop-down menu, Yes or No? And PHY ID should be 00?

Q2:
At USB-2-MDIO Software Tool, when reading TDR_CFG1 Register(Address=x300), the following settings are correct?
PHY ID: 00
Extended Address: No
Register Address: 0300

Q3:
At USB-2-MDIO Software Tool, when reading dsp_reg_72 Register(Address=x872), the following settings are correct?
PHY ID: 00
Extended Address: Tes
Register Address: 0872

Best regards

K.Hirano

  • Hello,

    Let me correct my typo at Q3:

    Q3:
    At USB-2-MDIO Software Tool, when reading dsp_reg_72 Register(Address=x872), the following settings are correct?
    PHY ID: 00
    Extended Address: Yes
    Register Address: 0872

    Best regards,

    K.Hirano

  • Hi Hirano, 

    Q1:
    At DP83TD510E-EVM, which should be selected at the Extended Register drop-down menu, Yes or No? And PHY ID should be 00?

    If you are trying to read a register that is a part of the default register set, i.e, registers 0x00-0x1F, then you would need to select "No". For any other registers after 0x1F, it would need to be "Yes". The PHY ID should be the PHY ID of the device whose registers you are trying to access. For the 510EVM, there are 2 such devices, the 510 itself, with PHY ID = 00, and the DP83822, with PHY ID = 05.

    At USB-2-MDIO Software Tool, when reading TDR_CFG1 Register(Address=x300), the following settings are correct?
    PHY ID: 00
    Extended Address: No
    Register Address: 0300

    No, since 0x300 is an extended register, extended address must be selected as "Yes"

    Q3:
    At USB-2-MDIO Software Tool, when reading dsp_reg_72 Register(Address=x872), the following settings are correct?
    PHY ID: 00
    Extended Address: Tes
    Register Address: 0872

    Yes, this would be correct. 

    Best,

    Vivaan