Hello,
We need an isolated CAN transceiver which also features 'hot-plug'. But I cannot find one within the isolated CAN transceiver category.
After some research into the existing the product which marked as 'hot-plug capable' such as TCAN-1642 , I realize that hot -plug capable CAN transceiver has the following features:
- power up/down glitch free operation on bus and RXD output
- Ideal passive, high impedance bus terminals when unpowered
1. Can I say that any TI CAN transceiver with above two features equivalent to 'hot-plug capable' ?
2. I found in the datasheet of ISO1042 also has the above two features. Does that mean ISO 1042 is 'hot-plug capable'?
Thanks