The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO1212: ISO1212 IPC-2221 Clearance Requirements

Part Number: ISO1212
Other Parts Discussed in Thread: ISO1211

Pins between ISO1212 are 0.225mm apart. What does TI recommend to comply with IPC-2221 Table 6-1 for uncoated lands and leads? 

Pin voltage between IN1 and FGND1 can be as high as 60VDC per the datasheets. This corresponds with a pin spacing of 0.5mm.