Tool/software:
Hello
1. I want to use ISO1228 and i don't need the visual indication & wants to LEDx direct to the ground but i read in section 7.3.2
"The LEDx pins can be connected directly to GND in sink mode provided wire-break detection is not used and V24V in source mode."
so if i connect LEDx direct to GND in sink mode, i lost the wire-break detection. Am i right? i really interested how happen is this? i can't figure it out from Block diagram Fig 7.1.
if just voltage drop on led is concerned, can i replace it with a resistor with same voltage drop once input is high?
2. the second question is about the equations in datasheet and the fixed number in that. where is the origin of this number? how is calculated?
for example in equation for wire break detection RIWB = (VINX -2V) /IWB - RTHR. what is the reference of 2v? is it voltage drop on LED and if i connect direct LED to GND this eqation is not valid?
or other equation on section 8.2.3.1.1
VIH (typical) = 6.0 V + RTHR x IL (typical) (2)
VIL (typical) = 5.0 V + RTHR x IL (typical) (3)
VIH (max) = 6.4 V + RTHR x IL (max) (4)
VIL (min) = 4.7 V + RTHR x IL (min) (5)
how calculated the numbers of 6, 5, 6.4, 4.7?
Thanks