Due to the U.S. Thanksgiving holiday, please expect delayed responses during the week of 11/22.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO1212: use in TPS2373's TPH/TPL/BT pin to isolate LED

Part Number: ISO1212
Other Parts Discussed in Thread: TPS2373, , ISO1211

Dear expert,

My customer uses our TPS2373 and TPL/TPH/BT pins LED indicator need to be isolated. But TPS2373 datasheet (P33) suggest them to use photos to isolate. Could you please help check if ISO121x is suitable for this application? If yes, could you help provide the reference circuit including the connection and Rthr and Rsense value. Very appreciate your help.

P.S Vc is 12V.

Regards,

Polly Chung