There are 3pins need to clear:
Pin 1 (Strobe) when high will push the inputs directly to the outputs, but when it goes low it will hold the previously applied output in the display.
Is it mean 4 bit input pin directly to a~g output pins?
Pin 6 (DIS FEQ IN) when high the output led will be treated as active low however when low the outputs will be active high
If our 7 segment display LED is common anode, then pin 6 should be high?
Pin 7 (VEE) Will be the low value of the output If tied to ground when outputs are low they will be 0V
Is it mean when VEE is 1V, then output Low is 1V?
And for input these pins for High, should we add Pull high resistor?
Thanks