Dear Sir:
SN74AUP1G97 FUNCTION Issue.
Input A of SN74AUP1G97 : High.
Input B of SN74AUP1G97 : High.
Input C of SN74AUP1G97 : Low.
Output Y of SN74AUP1G97 : High.
When the input C changes from Low to High.
Whether it will cause the Output Y of SN74AUP1G97 abnormally?
1. When the input C changes from Low to High.
The Output Y of SN74AUP1G97 abnormally.
The Output Y of SN74AUP1G97 will have the drop down from high to Low, and then up from low to high.
Does it happen the abnormal Phenomenon Output Y of SN74AUP1G97 ?
2. When the input C changes from Low to High.
The Output Y of SN74AUP1G97 normally.
The Output Y of SN74AUP1G97 will not have the drop down from high to Low, and then up from low to high.
The Output Y of SN74AUP1G97 will keep high always normally ( no drop down ) when the input C changes from Low to High.
Is it correct?
Please check to reply us asap.
Thanks a lot.
Best regards,
Vincent