The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Is 3.3V pullup required on CB3T bus switch outputs?

Other Parts Discussed in Thread: SN74CB3T16211

Is 3.3V pullup required in CB3T family of devices (sn74cb3t16211 - 24 bit). we are using this device with VCC of 3.3V to translate 5V swing signals to 3.3v swing signals on a CPCI interface. In fact, the input signals to sn74cb3t16211 could be either of 5V or 3.3v swing. Signals would be of maximum 33 MHz.

The following is from the datasheet of sn74cb3t16211:

" The I/O port of this device has a pullup current source that maintains the output voltage at VCC when the device is ON, and the input is greater than or equal to VCC – 1. Because of the pullup current source, the output voltage level may be less than VCC when the operating frequency is low and the I/O port is connected to a pulldown resistor. In order to maintain the output voltage at VCC, a pullup resistor must be connected to VCC instead of a pulldown resistor to ground. "

Thank you.