The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74S244: Logic compatibility

Part Number: SN74S244
Other Parts Discussed in Thread: SN74LVC8T245

In datasheet mention that it will accept 2.5 and 3.3V logic inputs. Can you please confirm it will accept LVCMOS/LVTTL/HCMOS as an inputs? 

Also confirm the part status, EOL, Lead time of this part number?

  • Hello,

    In datasheet mention that it will accept 2.5 and 3.3V logic inputs. Can you please confirm it will accept LVCMOS/LVTTL/HCMOS as an inputs? 

    Also confirm the part status, EOL, Lead time of this part number?

    The SN74S244 supports TTL and TTL-compatible input signals, specifically with VIH of 2V or more, and VIL of 0.8V or less. It has an input current requirement of up to

    As for availability, you can find which packages are available on the TI website:

    Our EOL policy can be found here: [FAQ] When will TI End of Life (EOL) or Obsolete a certain logic device?

    --

    Can you tell me more about your application? For example, loading, data rates, operating voltages, rails available in the system... any information is helpful to select a part.

    The "S" family of logic is quite old, and I would usually not recommend to use it in a modern design.  There are typically many better options. It sounds like you don't know what voltage signals are going to be in your system -- is this some kind of universal voltage translation requirement? Do you need the 64mA sink current of the "S" family?

    The best solution will most likely be a dual supply voltage translator like the SN74LVC8T245, which allows for up or down translation from 1.65V up to 5.5V, or any values in-between.

  • Thank you for your reply.

    Yes, I need 64mA sink current part for this application. 

    I am generating 32MHz, 16MHz and 8MHz clock form 3.3V(LVCMOS logic) PLL and I have to provide this clocks to DSP, which works at 5V (TTL/CMOS logic).

    Please confirm can we use "SN74LVC8T245" part to convert the clocks from 3.3V to 5V and vice-versa?

  • I'm surprised to hear that a modern DSP was designed to work with TTL signals and that it requires 64mA of drive current -- that's quite unusual.

    The LVC logic device will not drive a 64mA load, however it will support 32 MHz clock redriving without any problems with a 50pF load. You can do up or down translation from 3.3V to 5V with an LVC translator.

  • Thank you for your reply.

    FYI, This DSP part is a older one and we are decided to go with the old part.