Other Parts Discussed in Thread: TMS570LC4357
We are using RM57/TMS570LC4357 in a product and we are testing ram swap feature to understand if it can be helpful for us..
We are able to run a ram app different from the main flash app using the CPU_RESET method after swapping RAM/FLASH addresses. The only change we need to do is to reconfigure pinmux.
The ram app is able to relaunch the main flash app through a cold reset, done via SYSECR (Global System reset). Is this assumption correct? We tested also watchdog reset via WDKEY.
Do the RM57 got true hardware reset after the Global System reset?
Is there any information about RM57 register/module issue after a SYS_RESET or a WDOG_RESET?
Regards
Luciano