Part Number: TM4C1231H6PM
Hi There,
We are using TM4C1231H6PM controller on custom board. Initially we have created an application and able to run the same on custom board. Then we integrated FreeRTOS with CMSIS RTOS2 and verified the integration using TI TM4C123GH6 EVK board. Then we tried to download the same FW into custom board(with TM4C1231H6PM). After successfully downloading, IAR stuck in not responding mode and then we did not able to download the FW on subsequent tries. We tried these on multiple board, but the issue is same. Now even old FW is not working for those boards. We tried to erase the memory using JFlash but the tool is not able to connect with CPU.
Can somebody help?
MCU - TM4C1231H6PM
IDE - IAR 9.30
Debugger - J-link