The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM2434: After configuring the Timer according to the set period, clock jitter occurs during actual testing in the AM2434.

Part Number: AM2434

Background: Find this problem used the SDK version is the mcu_plus_sdk_am243x_08_05_00_24;

Question1:

1. When using TIME2 as the timer clock for interrupt 8k in the R50-0 core, testing revealed jitter phenomena of 125us, 126us, and even 124us.

The configuration of the Timer2 shown as followed:

So why the jitter occurred?

Question2:

I found that the cycle calculation of the timer in the latest version of the MCU_SDK, which is mcu_plus_sdk_am243x_09_01_00_41, is different from the one I used, which is 243x_08_05_00_24. I would like to ask why such changes were made.

The interface TimerP_setup defined in the TimeP.c of the two version:

Question 3:

Would the changes in problem 2 be a solution to problem 1???