LP-AM243: OSPI Bootloader Example Issue

Part Number: LP-AM243
Other Parts Discussed in Thread: SYSCONFIG, UNIFLASH

Tool/software:

MCU-PLUS-SDK 10.0.0

Example: sbl_ospi_am243x-lp_r5fss0-0_nortos_ti-arm-clang

If I compile the above example, with its default sysconfig settings (specifically "Application Image is X509 Signed"=ON & "Disable Auth For Application Image"=OFF), and flash it to OSPI then it always fails to boot my system image.

If I use the mcu_plus_sdk_am243x_10_00_00_20/tools/boot/sbl_prebuilt/am243x-lp/sbl_ospi.debug.hs_fs.tiimage prebuilt bootloader then my system image boots fine.

Example sysconfig settings:

I have debugged the bootloader, below is the call stack, and the line it fails on.

When this line is hit, I get a data abort.

Please pay attention to pSrc / pDst of the memcpy.

Note: For debugging purposes I can put a Flash_read() statement that reads flash offset 0x80000 and does not cause a data abort. I am therefore thinking 0x80000 in pDst is not a valid destination for the memcpy? 

Please can you advise on this problem. I am currently developing a custom bootloader where I also run into this same problem.

Is the prebuilt SBL bootloader compiled with certificate auth turned off? Is this related to the problem, or is something else going on?

  • Hi,

    Thanks for your patience.

    Allow me sometime to read through the detailed question and get back to you once I have further updates.

    Regards,

    Vaibhav

  • Hi,

    Can you try to put the destination buffer in MSRAM?

    Please read more here: https://software-dl.ti.com/mcu-plus-sdk/esd/AM64X/latest/exports/docs/api_guide_am64x/MEMORY_MAP.html

    Regards,

    Vaibhav

  • I am using the SBL_OSPI example from SDK 10.0.0.

    I notice from SDK version 10.0.0-> 10.0.1 this buffer (and supporting code) is added to main.c in the SBL_OSPI example.

    So I assume this is the buffer you'd like me to setup?

    My system image is 815Kib, so the buffer would need to be placed in an area of MSRAM where the code will be loaded. Will that be a problem?

    Can you share the source for the sbl_ospi.debug.hs_fs.tiimage prebuilt bootloader? I would like to know how it is different and why it works, when the example needs modification?

  • Hi,

    Can you share the source for the sbl_ospi.debug.hs_fs.tiimage prebuilt bootloader?

    Source is inside MCU_PLUS_SDK_INSTALL_PATH/examples/drivers/boot/sbl_ospi.

    Please read more about it here: https://software-dl.ti.com/mcu-plus-sdk/esd/AM243X/10_01_00_32/exports/docs/api_guide_am243x/EXAMPLES_DRIVERS_SBL_OSPI.html

    So I assume this is the buffer you'd like me to setup?

    That is correct. I checked the .app section in the file named sbl_ospi.release.map.

    It is allocated under MSRAM, so you have to make sure your destination buffer is in MSRAM in this case.

    Regards,

    Vaibhav

  • Moreover, please note the following:

    In the latest SDK that is 10.01.00.32

    in the file: ospi_lld.h

    If you see how OSPI_NOR_PROTOCOL is defined:

    #define OSPI_NOR_PROTOCOL(cmddataaddrdtr) (uint32_t)(((uint32_t)(dtr) << 24| \
                                                            ((uint32_t)(cmd) << 16| \
                                                            ((uint32_t)(addr) << 8| \
                                                            ((uint32_t)(data) << 0))
    It is wrongly mentioned, so it should be written as:
    #define OSPI_NOR_PROTOCOL(cmd, addr, datadtr) (uint32_t)(((uint32_t)(dtr) << 24| \
                                                            ((uint32_t)(cmd) << 16| \
                                                            ((uint32_t)(addr) << 8| \
                                                            ((uint32_t)(data) << 0))
    Notice, how I swapped the addr and data, because when you say a protocol like xS-yS-zS then x lines are used for command, y lines are used for address and z lines are used for data.
    So please do the changes as I have shown.
    And then simply build the driver libraries again by going to command prompt:

  • I'm a little confused, if the source for the sbl_ospi.debug.hs_fs.tiimage prebuilt image is exactly the same as examples/drivers/boot/sbl_ospi.. then why when I build the completely unmodified example, do I have this problem? Can you explain?

    I can try your suggestions in the next couple of days.

  • Hi Toby,

    I'm a little confused, if the source for the sbl_ospi.debug.hs_fs.tiimage prebuilt image is exactly the same as examples/drivers/boot/sbl_ospi.. then why when I build the completely unmodified example, do I have this problem? Can you explain?

    Is your question more of the booting works when using SBL_OSPI default SDK prebuilt images and fails to work when you use the newly built image without modifying the application at all.

    If yes, please tell me the steps how you are trying to run the application SBL_OSPI?

    Regards,

    Vaibhav

  • OK, bear in mind I'm testing this with SDK 10.0.0.

    So, prebuilt SBL image works fine.

    I import the sbl_ospi example into CCS and build it without any changes to the code.

    I set the AM243x-LP to UART boot and use the CLI version of uniflash with below config file.

    I set the AM243x-LP to OSPI boot. It fails to boot.

    uniflash config:

    The call stack in the screenshots on my first post are from the example, with the only change being that I put the call to loop_forever() at the start so I could connect the debugger while the bootloader was running.

  • Hi Toby,

    Thanks for your patience.

    CLI version of uniflash with below config file

    Do you mean to say using the uart_uniflash.py script which incorporates Python commands?

    The call stack in the screenshots on my first post are from the example, with the only change being that I put the call to loop_forever() at the start so I could connect the debugger while the bootloader was running.

    Inside SBL_OSPI I have seen where you are seeing data abort error.

    Let me follow the same steps as you are doing and see if I can come to a same point as yours.

    Regards,

    Vaibhav

  • Do you mean to say using the uart_uniflash.py script which incorporates Python commands?

    Correct, command below.

    Fullscreen
    1
    python c:/ti/mcu_plus_sdk_am243x_10_00_00_20/tools/boot/uart_uniflash.py -p COM13 --cfg=sbl_ospi_debug.cfg
    XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

    Let me follow the same steps as you are doing and see if I can come to a same point as yours.

    This is a good plan.

    Other information that may be relevant: the application I am flashing is generated by a system project and contains images for both cores of the first R5.

    The application .hs_fs image file is 816KB.

  • Hi,

    I have checked your screenshot.

    I am assuming it was from file main.c for SBL OSPI.

    On this note: 

    For me I do not see the call to Flash_imgOffsetRead inside Flash_imgOpen

    But in your screenshot how come do you have this call?

    Can you explain?

    Regards,

    Vaibhav

  • Can you explain?

    You're looking at SDK version 10.0.1 and I'm using SDK version 10.0.0.

  • I am looking at 10.0 itself:

    I see both 10.0 and 10.01 has the same definition:

  • I'm going to reinstall mcu_plus_sdk_10.0.0 and check again.

  • I've re-installed the SDK and that function call is not present.

    I can only assume that we modified bootloader_flash.c at some point during development / testing.

    I will rebuild the bootloader and test again and let you know if it works. This will be in the next couple of days.

    Thank you for your patience.

  • I've re-installed the SDK and that function call is not present.

    I can only assume that we modified bootloader_flash.c at some point during development / testing.

    I will rebuild the bootloader and test again and let you know if it works. This will be in the next couple of days.

    Thank you for your patience.

    Thanks for reinstalling.

    It must be that one of the developers must have modified the API to debug some functionality.

    Either way it should work with both the SDKs.

    Let me know how it goes.

    Looking forward to your response.

    Thanks,

    Vaibhav

  • Thanks for your help. Issue resolved.

  • Hi Toby,

    Glad to know that the issue has been resolved.

    Marking this thread closed, please raise another e2e for further questions/doubts.

    Looking forward to help you out Slight smile

    Regards,

    Vaibhav