Other Parts Discussed in Thread: TMS320F28335
Dear Sir,
I am using a TMS320F28335 to implement a control for 3 phase active front end converter. When i starts the code it works fine but the moment i turn on the mains(3-ph) voltage to the converter. CCS expression window freezes and after sometime GEL expression window pops up for every expression i have in the expression window. Once that is over either the following error comes or CCS stops responding.
Error:
C28xx: Error: (Error -1041 @ 0xFFFFFF6A) The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 9.4.0.00129)
C28xx: Trouble Halting Target CPU: (Error -2062 @ 0x0) Unable to halt device. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 9.4.0.00129)
C28xx: Error: (Error -1041 @ 0xFFFFFF6A) The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 9.4.0.00129)
C28xx: Trouble Halting Target CPU: (Error -150 @ 0x0) One of the FTDI driver functions used during configuration returned a invalid status or an error. (Emulation package 9.4.0.00129)
C28xx: Unable to determine target status after 20 attempts
C28xx: Failed to remove the debug state from the target before disconnecting. There may still be breakpoint op-codes embedded in program memory. It is recommended that you reset the emulator before you connect and reload your program before you continue debugging
Please let me know if you need more information.
Thanks,
Shubham Dhiman