Part Number: TMS320F28388D
Dear all,
For a flash build C28x-CLA1 program , i came to an understanding that bfore we run cla we need to copy cla programs to configured memory RAM .This copy using memcpy() function is earlier seen by using pragma command to specify to which section of flash the code should reside and to which portion of ram we will load it while running . But in CLA example for epwm i cannot find usage of Ca1Prog section specification in .cla source file.
How we are loading cla code into Ls ram ?. Should nt we specify the section by some method like
__interrupt void cpuTimer0ISR(void);
#pragma CODE_SECTION(cpuTimer0ISR, "isrfunc")
in the above code we are specifying isrfunc section for timerisr function.
and this linker words will make it run. at RAMGS15
isrfunc : LOAD = FLASH0| FLASH1,
RUN = RAMGS15,
LOAD_START(isrfuncLoadStart),
LOAD_END(isrfuncLoadEnd),
RUN_START(isrfuncRunStart),
LOAD_SIZE(isrfuncLoadSize)
but am not able to find any such method of pragma usage for the Cla1Prog section in the pwm cla example in c2000 .
how the compiler comes to know it should keep the functions in .cla source file in FLASH4 only
Cla1Prog : LOAD = FLASH4,
RUN = RAMLS5,
LOAD_START(Cla1funcsLoadStart),
LOAD_END(Cla1funcsLoadEnd),
RUN_START(Cla1funcsRunStart),
LOAD_SIZE(Cla1funcsLoadSize),
ALIGN(8)
also please give an idea on following code from cmd file
/* CLA C compiler sections */
//
// Must be allocated to memory the CLA has write access to
//
CLAscratch :
{ *.obj(CLAscratch)
. += CLA_SCRATCHPAD_SIZE;
*.obj(CLAscratch_end) } > RAMLS1
.scratchpad : > RAMLS1
.bss_cla : > RAMLS1
cla_shared : > RAMLS1
#if defined(__TI_EABI__)
.const_cla : LOAD = FLASH2,
RUN = RAMLS1,
RUN_START(Cla1ConstRunStart),
LOAD_START(Cla1ConstLoadStart),
LOAD_SIZE(Cla1ConstLoadSize)
#else
.const_cla : LOAD = FLASH2,
RUN = RAMLS1,
RUN_START(_Cla1ConstRunStart),
LOAD_START(_Cla1ConstLoadStart),
LOAD_SIZE(_Cla1ConstLoadSize)
Thanks and regards,
Stevin Martin
CLA_SCRATCHPAD_SIZE = 0x100;
--undef_sym=__cla_scratchpad_end
--undef_sym=__cla_scratchpad_start
MEMORY
{
/* BEGIN is used for the "boot to Flash" bootloader mode */
BEGIN : origin = 0x080000, length = 0x000002
BOOT_RSVD : origin = 0x000002, length = 0x0001AF /* Part of M0, BOOT rom will use this for stack */
RAMM0 : origin = 0x0001B1, length = 0x00024F
RAMM1 : origin = 0x000400, length = 0x0003F8 /* on-chip RAM block M1 */
// RAMM1_RSVD : origin = 0x0007F8, length = 0x000008 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
RAMD0 : origin = 0x00C000, length = 0x000800
RAMD1 : origin = 0x00C800, length = 0x000800
RAMLS0 : origin = 0x008000, length = 0x000800
RAMLS1 : origin = 0x008800, length = 0x000800
RAMLS2 : origin = 0x009000, length = 0x000800
RAMLS3 : origin = 0x009800, length = 0x000800
RAMLS4 : origin = 0x00A000, length = 0x000800
RAMLS5 : origin = 0x00A800, length = 0x000800
RAMLS6 : origin = 0x00B000, length = 0x000800
RAMLS7 : origin = 0x00B800, length = 0x000800
RAMGS0 : origin = 0x00D000, length = 0x001000
RAMGS1 : origin = 0x00E000, length = 0x001000
RAMGS2 : origin = 0x00F000, length = 0x001000
RAMGS3 : origin = 0x010000, length = 0x001000
RAMGS4 : origin = 0x011000, length = 0x001000
RAMGS5 : origin = 0x012000, length = 0x001000
RAMGS6 : origin = 0x013000, length = 0x001000
RAMGS7 : origin = 0x014000, length = 0x001000
RAMGS8 : origin = 0x015000, length = 0x001000
RAMGS9 : origin = 0x016000, length = 0x001000
RAMGS10 : origin = 0x017000, length = 0x001000
RAMGS11 : origin = 0x018000, length = 0x001000
RAMGS12 : origin = 0x019000, length = 0x001000
RAMGS13 : origin = 0x01A000, length = 0x001000
RAMGS14 : origin = 0x01B000, length = 0x001000
RAMGS15 : origin = 0x01C000, length = 0x000FF8
// RAMGS15_RSVD : origin = 0x01CFF8, length = 0x000008 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
/* Flash sectors */
FLASH0 : origin = 0x080002, length = 0x001FFE /* on-chip Flash */
FLASH1 : origin = 0x082000, length = 0x002000 /* on-chip Flash */
FLASH2 : origin = 0x084000, length = 0x002000 /* on-chip Flash */
FLASH3 : origin = 0x086000, length = 0x002000 /* on-chip Flash */
FLASH4 : origin = 0x088000, length = 0x008000 /* on-chip Flash */
FLASH5 : origin = 0x090000, length = 0x008000 /* on-chip Flash */
FLASH6 : origin = 0x098000, length = 0x008000 /* on-chip Flash */
FLASH7 : origin = 0x0A0000, length = 0x008000 /* on-chip Flash */
FLASH8 : origin = 0x0A8000, length = 0x008000 /* on-chip Flash */
FLASH9 : origin = 0x0B0000, length = 0x008000 /* on-chip Flash */
FLASH10 : origin = 0x0B8000, length = 0x002000 /* on-chip Flash */
FLASH11 : origin = 0x0BA000, length = 0x002000 /* on-chip Flash */
FLASH12 : origin = 0x0BC000, length = 0x002000 /* on-chip Flash */
FLASH13 : origin = 0x0BE000, length = 0x001FF0 /* on-chip Flash */
// FLASH13_RSVD : origin = 0x0BFFF0, length = 0x000010 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
CPU1TOCPU2RAM : origin = 0x03A000, length = 0x000800
CPU2TOCPU1RAM : origin = 0x03B000, length = 0x000800
CPUTOCMRAM : origin = 0x039000, length = 0x000800
CMTOCPURAM : origin = 0x038000, length = 0x000800
CANA_MSG_RAM : origin = 0x049000, length = 0x000800
CANB_MSG_RAM : origin = 0x04B000, length = 0x000800
RESET : origin = 0x3FFFC0, length = 0x000002
CLA1_MSGRAMLOW : origin = 0x001480, length = 0x000080
CLA1_MSGRAMHIGH : origin = 0x001500, length = 0x000080
}
SECTIONS
{
codestart : > BEGIN, ALIGN(8)
.text : >> FLASH1 | FLASH2 | FLASH3 | FLASH4, ALIGN(8)
.cinit : > FLASH1, ALIGN(8)
.switch : > FLASH1, ALIGN(8)
.reset : > RESET, TYPE = DSECT /* not used, */
.stack : > RAMM1
#if defined(__TI_EABI__)
.init_array : > FLASH1, ALIGN(8)
.bss : > RAMLS3
.bss:output : > RAMLS3
.data : > RAMLS4
.sysmem : > RAMLS4
/* Initalized sections go in Flash */
.const : > FLASH5, ALIGN(8)
#else
.pinit : > FLASH1, ALIGN(8)
.ebss : > RAMLS3
.esysmem : > RAMLS4
/* Initalized sections go in Flash */
.econst : >> FLASH4 | FLASH5, ALIGN(8)
#endif
MSGRAM_CPU1_TO_CPU2 : > CPU1TOCPU2RAM, type=NOINIT
MSGRAM_CPU2_TO_CPU1 : > CPU2TOCPU1RAM, type=NOINIT
MSGRAM_CPU_TO_CM : > CPUTOCMRAM, type=NOINIT
MSGRAM_CM_TO_CPU : > CMTOCPURAM, type=NOINIT
dclfuncs : > FLASH1, ALIGN(8)
/* CLA specific sections */
#if defined(__TI_EABI__)
Cla1Prog : LOAD = FLASH4,
RUN = RAMLS5,
LOAD_START(Cla1funcsLoadStart),
LOAD_END(Cla1funcsLoadEnd),
RUN_START(Cla1funcsRunStart),
LOAD_SIZE(Cla1funcsLoadSize),
ALIGN(8)
#else
Cla1Prog : LOAD = FLASH4,
RUN = RAMLS5,
LOAD_START(_Cla1funcsLoadStart),
LOAD_END(_Cla1funcsLoadEnd),
RUN_START(_Cla1funcsRunStart),
LOAD_SIZE(_Cla1funcsLoadSize),
ALIGN(8)
#endif
CLADataLS0 : > RAMLS0
CLADataLS1 : > RAMLS1
Cla1ToCpuMsgRAM : > CLA1_MSGRAMLOW, type=NOINIT
CpuToCla1MsgRAM : > CLA1_MSGRAMHIGH, type=NOINIT
Cla1DataRam : >> RAMLS0 | RAMLS1
/* CLA C compiler sections */
//
// Must be allocated to memory the CLA has write access to
//
CLAscratch :
{ *.obj(CLAscratch)
. += CLA_SCRATCHPAD_SIZE;
*.obj(CLAscratch_end) } > RAMLS1
.scratchpad : > RAMLS1
.bss_cla : > RAMLS1
cla_shared : > RAMLS1
#if defined(__TI_EABI__)
.const_cla : LOAD = FLASH2,
RUN = RAMLS1,
RUN_START(Cla1ConstRunStart),
LOAD_START(Cla1ConstLoadStart),
LOAD_SIZE(Cla1ConstLoadSize)
#else
.const_cla : LOAD = FLASH2,
RUN = RAMLS1,
RUN_START(_Cla1ConstRunStart),
LOAD_START(_Cla1ConstLoadStart),
LOAD_SIZE(_Cla1ConstLoadSize)
#endif
#if defined(__TI_EABI__)
.TI.ramfunc : {} LOAD = FLASH3,
RUN = RAMD0,
LOAD_START(RamfuncsLoadStart),
LOAD_SIZE(RamfuncsLoadSize),
LOAD_END(RamfuncsLoadEnd),
RUN_START(RamfuncsRunStart),
RUN_SIZE(RamfuncsRunSize),
RUN_END(RamfuncsRunEnd),
ALIGN(8)
#else
.TI.ramfunc : {} LOAD = FLASH3,
RUN = RAMD0,
LOAD_START(_RamfuncsLoadStart),
LOAD_SIZE(_RamfuncsLoadSize),
LOAD_END(_RamfuncsLoadEnd),
RUN_START(_RamfuncsRunStart),
RUN_SIZE(_RamfuncsRunSize),
RUN_END(_RamfuncsRunEnd),
ALIGN(8)
#endif
}
/*
//===========================================================================
// End of file.
//===========================================================================
*/