Hi experts,
My customer is using IEC60730 safety lib, and they split the flash to about 100 blocks and do the flash self-test one by one. Now, the whole Flash self-test needs about 90 seconds, they want to decrease to 45 seconds or less.
I find the benchmarks in IEC60730_F2803x_STL_User_Manual, it show as below:
So, if we use STL_CRC_TEST_testNvMemory to test the whole Flash, how long it lasts? Does splitting the Flash into too many blocks lead to the too long self-test time?
Thanks and regards,
Jim