Other Parts Discussed in Thread: UNIFLASH,
Hi,
I am struggling with the verification hex file issue in UniFlash (ver.8.4.0.4458) for Arm core (TMS320F28388D)
Description:
- In CCS there is no error after compilation, the program can be downloaded and is started properly.
- In UniFlash after .hex file verification I get the message: "File Loader: Verification failed: Values at address 0x200000@Program do not match Please verify target and memory map". Nevertheless the program can be downloded but doesn't start.
When I make the verification for .out file I have the same message but I can also download and the program is started properly.
I have attached:
- a snapshot from UniFlash
- a debug folder with .hex and .out file