Part Number: TMS320F28P650DH
Tool/software:
We are using TMS320F28P650DH.
There is strange behavior when use TBPHS to achieve phase shift function.
we take epwm_ex3_synchronization for reference.
EPWM1 create sync out pulse. EPWM2 sync in source is EPWM1 sync out signal. UP counter mode Period: 2000 (200M system clock)
EPWM2 epwm2A -> 0 set high, compA set low. epwm2B -> compA set high compB set low.
Some condition is normal.
But there are two condition that have abnormal behavior. EPWM2A is always high and EPWM2B is always low.
1. compA value < TBPHS.
2. compA value>TBPHS and TBPHS is < 10% period.
We are debugging HW, it is urgent. Thank you for your help.