Other Parts Discussed in Thread: C2000WARE
Hi,
I have been working on a project that I am hoping to use the Digital Controller Library (DCL). I have followed the directions of the user guide SPRUI31 and the project builds, but the moment a DCL function is called, the program crashes.
I have been using the PSFB project in C2000Ware as a reference to help me understand what is happening and I noticed something interesting when looking at the disassembly. In the reference project, the disassembly matches the .asm files of the DCL. In my project however, an ITRAP0 instruction is present between every single line. Below I have a screen capture of both cases. Any idea what could cause such as difference?
I am running both projects in the same hardware on a F280049 with the same XDS200. I am using the same version of CCS (10.1.1.00004), compiler (TI v20.2.1.LTS).
Any help or suggestions that can point me in the right direction is really appreciated.
Best regards,
Luccas