Other Parts Discussed in Thread: MSP430-FLASHER, , MSP-EXP430F5438
**This is an informative post and all replies will be ignored. If you have questions or issues, please make a new E2E post and reference this one. Thank you. **
There is a known issue when using MSP-FETs with serial number starting with the digits "17" or greater with versions of CCS below v7.0, IAR EW430 v7.1 and IAR EWARM v8.10. The issue can also affect old versions of the MSP430-Flasher (in this case update to the latest version). The issue can exhibit as a "Could not set device Vcc" error message or other error messages. This is because these older versions of the IDEs were released before this latest version of the MSP-FET tool, and therefore do not recognize and handle the new tools correctly.
The preferred solution is to update to the latest version of CCS or IAR. However, if updating is not an option in your case, please install the appropriate patch for your CCS or IAR version. The table summarizes version compatibility and available patches:
New MSP-FET (Serial number starting "17" or greater) | Older MSP-FET (Serial number starting less than "17") | |
CCS v6.0 or earlier | Not Supported | Supported |
CCS v6.1.2 | 6406.CCS_6_1_2.zip | Supported |
CCS v6.1.3 | CCS_6_1_3.zip | Supported |
CCS v6.2 | CCS_6_2.zip | Supported |
CCS v7.0 or greater | Supported | Supported |
New MSP-FET (Serial number starting "17" or greater) | Older MSP-FET (Serial number starting less than "17") | |
IAR EW430 v6.40.1 or earlier | Not Supported | Supported |
IAR EW430 v6.40.2 through IAR EW430 v7.0 | IAR.zip | Supported |
IAR EW430 v7.1 or greater | Supported | Supported |