The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C129XNCZAD: 'Timer Compare Action Mode': output pin is not affected at compare match time

Part Number: TM4C129XNCZAD
Other Parts Discussed in Thread: TM4C129CNCZAD, , SEGGER

Hello,

we have an issue using the ‘Timer Compare Action Mode’ on the TM4C microcontroller and hope you can support us. The connected output pin is not affected at compare match time.

Ambient conditions:

  • Target controller: TM4C129CNCZAD
  • Currently used controller: TM4C129XNCZAD on DK-TM4C129X evaluation board
  • Compiler: IAR Embedded Workbench for ARM 9.10.2.39460

Use case:

To control our physical process, we need several timers in combination with timer compare action mode to switch digital outputs at defined times in the future without processor action.

  • Timer A and B are use individual in 16-bit mode
  • Timers are configured as periodic with a timer interval load of 0xFFFF. Timers are free running and cannot be reinitialized during normal operation.
  • Digital output must only be switched at compare time. Timer timeout must not affect the digital output. The physical process is asynchronous to the timer period.

Used configuration:

  • TCACT in GPTMTnMR register is set to a non-zero value to configure the pin switching.
  • TnAMS bit is set to zero: Capture or compare mode is enabled.
  • For switching the output GPTMTnMATCHR register is set with the time for next switching.
  • Timer interrupt is configured for timer-match interrupt
  • GPIOs are connected to the timer using the MUX.

Issue / current behaviour:

  • Timer match interrupt correctly occurs at compare match time. à OK
  • The corresponding output is not switched at compare match time. à not OK
  • The corresponding output is switched at timer timeout. à not OK
  • All non-zero values of TCACT do not lead to an output pin action at compare match time.

 Code extract:

void Timer1IntHandler(void)
{
    // this port switch is only for testing the timer match ISR
    GPIOPinWrite(GPIO_PORTQ_BASE, GPIO_PIN_3, GPIO_PIN_3);
    TimerIntClear(TIMER1_BASE, TIMER_TIMA_MATCH);
    GPIOPinWrite(GPIO_PORTQ_BASE, GPIO_PIN_3, 0);
}

int main(void)
{
    //
    // Run from the PLL at 120 MHz.
    // Note: SYSCTL_CFG_VCO_240 is a new setting provided in TivaWare 2.2.x and
    // later to better reflect the actual VCO speed due to SYSCTL#22.
    //
    ui32SysClock = SysCtlClockFreqSet((SYSCTL_XTAL_25MHZ |
                                           SYSCTL_OSC_MAIN |
                                           SYSCTL_USE_PLL |
                                           SYSCTL_CFG_VCO_240), 120000000);

    //
    // Configure the device pins.
    //
    PinoutSet();

    //
    // Enable the peripherals used by this example.
    //
    SysCtlPeripheralEnable(SYSCTL_PERIPH_TIMER1);

    //
    // Enable processor interrupts.
    //
    IntMasterEnable();

    TimerConfigure(TIMER1_BASE, TIMER_CFG_SPLIT_PAIR | TIMER_CFG_A_PERIODIC | TIMER_CFG_A_ACT_TOGGLE);
    
    TimerLoadSet(TIMER1_BASE, TIMER_A, 0xFFFF);
    TimerMatchSet(TIMER1_BASE, TIMER_A, 30000);

    IntEnable(INT_TIMER1A);
    
    TimerIntEnable(TIMER1_BASE, TIMER_TIMA_MATCH);

    GPIOPinConfigure(GPIO_PD2_T1CCP0);
    GPIOPinTypeTimer(GPIO_PORTD_BASE, GPIO_PIN_2);
    
    // configure output for ISR testing
    GPIOPinTypeGPIOOutput(GPIO_PORTQ_BASE, GPIO_PIN_3);
    GPIOPinWrite(GPIO_PORTQ_BASE, GPIO_PIN_3, 0);
       
    //
    // Enable the timers.
    //
    TimerEnable(TIMER1_BASE, TIMER_A);

    //
    // Loop forever while the timers run.
    //
    while(1)
    {
    }
}

We have the following questions:

  • Is it possible to configure Timer Compare Action Mode in such a way that only compare match affects the corresponding output pin? Timer timeout must not affect the output pin.
  • What error was made in the code sample so that the desired behaviour is not achieved.

 Thank you very much for your support.

 

Best regards,

Markus Karas

  • Hello Markus,

    I replicated your current situation and understand what you are trying to do. We will probably need to work this further next week to get a resolution here but I can explain what is going on with your current configuration.

    I am not 100% sure if it is possible to get the output to trigger on match and not timeout without manual GPIO control.

    Here is the details of the GPTMTAMR register on Page 1130 of the Device Datasheet. Specifically, this is for the TCACT (Timer Compare Action Select) register bits:

    Value Description

    0x0    Disable compare operations.
    0x1    Toggle State on Time-Out
    0x2    Clear CCP on Time-Out
    0x3    Set CCP on Time-Out
    0x4    Set CCP immediately and toggle on Time-Out
    0x5    Clear CCP immediately and toggle on Time-Out
    0x6    Set CCP immediately and clear on Time-Out
    0x7    Clear CCP immediately and set on Time-Out

    All of these indicate actions only on timeout and not on match and so the behavior makes sense based on this.

    I would need to dig deeper into how the match works for this to be sure, but it seems to me like the match won't trigger the toggling of the I/O, only an interrupt. And then in the interrupt you could handle the I/O toggle.

    It is a holiday weekend in the US so I will pick this back up on Tuesday, but may not have a reply back to you until Wednesday. Hopefully these initial details help you understand your observations at least.

    Best Regards,

    Ralph Jacobi

  • Hello Ralph,

    Thank you very much for this first assessment. Your description matches the debug results we made.

    In the manual on page 1114 our use case is described. Unfortunately we can't get the microcontroller to behave like that.

    Timer Compare Action Mode
    The timer compare mode is an extension to the GPTM's existing one-shot and periodic modes. This
    mode can be used when an application requires a pin change state at some time in the future,
    regardless of the processor state. The compare mode does not operate when the PWM mode is
    active and is mutually exclusive to the PWM mode. The compare mode is enabled when the TAMR
    field is set to 0x1 or 0x2 (one-shot or periodic), the TnAMS bit is 0 (capture or compare mode) and
    the TCACT field is nonzero in the GPTM Timer n Mode (GPTMTnMR) register. Depending on the
    TCACT encoding, the timer can perform a set, clear or toggle on the corresponding CCPn pin when
    a timer match occurs. In 16-bit mode, the corresponding CCP pin can have an action applied, but
    when operating in 32-bit mode, the action can only be applied to the even CCP pin.
    The TCACT field can be changed while the GPTM is enabled to generate different combinations of
    actions. For example, during a periodic event, encodings TCACT = 0x6 or 0x7 can be used to force
    the initial state of the CCPn pin before the first interrupt and following that, TCACT=0x2 and TCACT=0x3
    can be used (alternately) to change the sense of the pin for the subsequent toggle, while possible
    changing load value for the next period.
    The time-out interrupts used for one-shot and periodic modes are used in the compare action modes.
    Thus, the TnTORIS bits in the GPTMRIS register are triggered if the appropriate mask bits are set
    in the GPTMIM register.

    Tank you very much for your support.

    Best regards,

    Markus Karas

  • Hi Marcus,

    Have you checked the silicon errata PDF about timer actions? There are odd behaviors for match on upcount mode on some classes of MCU. 

    Regards,

  • Hi,

    thank you for the hint. We have already checked the errata. The listed topics do not correspond to the timer configuration used. We use periodic down counting timers, based on syclk.

    Best regards,

    Markus Karas

  • That's good you checked errata first and have you used CCS debug to confirm all timer registers being set as desired? 

  • We are using IAR Workbench combined with Segger's J-Trace. Yes, we have checked the registers to be correctly set according to the manual.

  • I don't see the timer control event being configured in your listed code. We use the interrupt edge event like Ralph mentions.

    /* Configure edge polarity capture events for CCP1. */
    MAP_TimerControlEvent(TIMER0_BASE, TIMER_A, TIMER_EVENT_POS_EDGE);

  • BTW: Seemingly CCP action events trigger is for GPIO captured events from package pins inward. Past experiments TM4C1294 never could get CCP pins to toggle a GPIO output to package pins. It's a capture event action for GPIO sense, not an output control action event.

  • Hello Markus,

    I agree that the description in the datasheet indicates that, but the registers seem to conflict with that which leaves me with doubt about if that functionality can actually be achieved. Unfortunately I was not able to spend much time on this today so I don't have any newer findings.

    Best Regards,

    Ralph

  • I guess TimerControlEvent() is only necessary in capture mode to define the edge to be captured. In compare mode this is not necessary in my opinion.

  • Hi Ralph,
    After all we have tried in the meantime, I think that the capture compare unit does not work as we need it to. Here the TM4C unfortunately differs from microcontrollers known so far.
    Nevertheless it would be very helpful if you can give me some feedback if something else has been found out in this regard.

    Thank you very much and best regards,
    Markus

  • You can force a timer to re-load well before time out event. Also in Oneshot mode the default reset match value is 32 bits wide, can be reduced to 0x1. The Oneshot mode can drive ADC sequencer trigger, perhaps even toggle CCPn pin on match count. 

        MAP_TimerClockSourceSet(TIMER1_BASE, TIMER_CLOCK_SYSTEM);
        MAP_TimerConfigure(TIMER1_BASE, TIMER_CFG_ONE_SHOT);
        /* Load the 32 bit Match value for one shot
         * re-load GPTMnMATCHR Reset value (FFFF.FFFF)  */
        MAP_TimerMatchSet(TIMER1_BASE, TIMER_A, 0x1);
        /* Set IMR interrupt disabled for timeout events */
        MAP_TimerIntDisable(TIMER4_BASE, TIMER_TIMA_TIMEOUT|TIMER_TIMA_MATCH);

  • Hello Markus,

    Okay so as far as "timer can perform a set, clear or toggle on the corresponding CCPn pin when a timer match occurs" goes, you need to use one of the these settings:

    • 0x4 Set CCP immediately and toggle on Time-Out
    • 0x5 Clear CCP immediately and toggle on Time-Out
    • 0x6 Set CCP immediately and clear on Time-Out
    • 0x7 Clear CCP immediately and set on Time-Out

    The problem is that this feature is not then setup to maintain that output. The signal will be toggled in some manner after the timeout. What I did find unusual is that instead of toggling on Time-Out, it toggled on the next Match set. So that behavior doesn't seem to line up with the exact register description, but I think in this case the datasheet isn't being explicit enough as the idea of needing to use other settings to toggle on timeout is mentioned explicitly:

    For example, during a periodic event, encodings TCACT = 0x6 or 0x7 can be used to force
    the initial state of the CCPn pin before the first interrupt and following that, TCACT=0x2 and TCACT=0x3
    can be used (alternately) to change the sense of the pin for the subsequent toggle, while possible
    changing load value for the next period.

    Digital output must only be switched at compare time. Timer timeout must not affect the digital output. The physical process is asynchronous to the timer period.

    As far as I can tell, you'll need to manually control the I/O via an interrupt of some sort. I'm not quite sure what to suggest for your system though because I don't know realistically what the other options are for you without the Match feature working as you had desired.

    Best Regards,

    Ralph Jacobi

  • Hello GI,

    we have also thought of manipulating the timer reload value to solve the issue. The problem of this solution is that we use 7 timers for switching different hardware signals. All these timers must run synchronous to have the same time base. So, we cannot manipulate the timer value or timer reload value of single timers.

    Thank you for your support.

    Best regards, Markus

      

    Hello Ralph,

    thank you for your assessment. We did not find a configuration for compare output which is suitable for our needs. We now use the compare match interrupt and control the output pins manually. We must check if the increased latency caused by the interrupt (or higher priority interrupts) influence our control algorithm.

    Thanks’ again for your support.

    Best regards,
    Markus

  • implemented in interrupt routine.

    solved and closed