I'm implementing a very minimal setup for the DRV8848 and I can't get it to output anything. Already tried a 50% PWM on AIN1 and low on AIN2, and just a HIGH and LOW on those pins. The fault and sleep pins are both high and all other voltages are within spec (7.2V on VM and 3.3V on VINT and VREF). I can see that all the outputs are grounded even without any load plugged in.
I've included my schematic and layout as well. I tried all troubleshooting steps I can think of, so any kind of help or ideas on what to check would be greatly appreciated.