Tool/software:
Hello,
While working on my design using the DRV8955, I noticed that the package for PWP and RGE differ slightly.
It seems that the PWP has two pins per output. I was just wondering why that was.
And to follow up - when using the MODE pin to adjust between the amount of solenoids being driven, are the pins paralleled internally or am I required to short them external to the chip? I would like to test multiple configurations and do not want to short it externally if I do not have to in order to reduce the amount of PCB revisions I do.
Regarding the H-bridge configuration, would I just be connecting the load between two OUTx pins?
Thanks in advance.