The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8874: Sensorless Speed Control (Ripple Counting)

Part Number: DRV8874
Other Parts Discussed in Thread: DRV8235

Tool/software:

I'm trying to use DRV8874 to control a 24V 5A DC motor.


However, it does not include sensorless speed control.


DRV8235 seems to be capable of sensorless speed control, but the current is 3.7A max.


Using DRV8874, can I make a Ripple Count function with an algorithm in MCU by High Speed ADC at IPROPI?


Is there a function that IPROPI's output can output Ripple?